Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design fpga programming using Ubuntu 18.04
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 355 subscribers
  • Views 1833 views
  • Users 0 members are here
  • mini-itx_hardware_design
Related

fpga programming using Ubuntu 18.04

amamory
amamory over 6 years ago

Hello,

 

I am testing a mini-itx board with Ubuntu 18.04 host OS.

 

The tests with builtin software went ok. However, when i try to program the FPGA via this module

https://store.digilentinc.com/jtag-smt2-surface-mount-programming-module/

 

The USB device is not even recognized. I checked with 'dmesg' command. Nothing changes when i plug the usb in or out.

 

It seems that there are 2 possibilities:

1) there is a special device driver for https://store.digilentinc.com/jtag-smt2-surface-mount-programming-module/

2) there is some jumper to allow jtag programming that I am missing.

 

Reading the manual, I see that SW7[1] enables the JTAG Cascaded. I switched this on and off and nothing changes. The USB port is not recognized.

 

So, what is necessary to have the USB JTAG working on Linux ?

 

best regards,

Alexandre

  • Sign in to reply
  • Cancel
Parents
  • amamory
    amamory over 6 years ago

    I just want to add that I have other boards, such as zedboard, and I can program them without problems. The issue I described earlier is related only with mini-itx board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • amamory
    amamory over 6 years ago

    I just want to add that I have other boards, such as zedboard, and I can program them without problems. The issue I described earlier is related only with mini-itx board.