Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design help me  with  usb hub problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 354 subscribers
  • Views 791 views
  • Users 0 members are here
Related

help me  with  usb hub problem

e14 Contributor
e14 Contributor over 10 years ago

In my board there is a usb hub device connected to the zynq PS usb controller, just like the mini-itx  board.
The issue confused meis that when running the linux kernel(3.14), it can not find the usb hub device, just prinf words like this:

hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected

when i input "lsusb" i can see "Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub ",but there should be usb hub device uunder root hub.

who can help me?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Just to be clear, are you using a Mini-ITX board or some other Zynq based board?

     

    If it is a Mini-ITX board which version are you using?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    thanks for your apply.
    I used a zynq based board.
    now the problem is
    "usb 1-1: new high-speed USB device number 2 using
    zynq-ehci
    usb 1-1: device not accepting address 2, error -71".
    is it caused by the hardware?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    thanks for your apply.
    I used a zynq based board.
    now the problem is
    "usb 1-1: new high-speed USB device number 2 using
    zynq-ehci
    usb 1-1: device not accepting address 2, error -71".
    is it caused by the hardware?