Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design PCIe addressing in Mini-ITX
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 354 subscribers
  • Views 524 views
  • Users 0 members are here
Related

PCIe addressing in Mini-ITX

e14 Contributor
e14 Contributor over 12 years ago


Hi,

I ahve a question about PCIe addressing in Mini-ITX.

Dose Mini-ITX support Large Block addressing for PCIe devices (larger than 4GB window)?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    In short, the answer is yes. The PCIe IP must be configured to support 64-bit addressing on the Endpoint device as well the Root Port running on the Mini-ITX board. The OS running on the Mini-ITX must support 64-bit addressing as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    In short, the answer is yes. The PCIe IP must be configured to support 64-bit addressing on the Endpoint device as well the Root Port running on the Mini-ITX board. The OS running on the Mini-ITX must support 64-bit addressing as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thank you,
    Is FPGA of ZYNQ in Mini-ITX (7Z100 SoC) is big enough to have a PCIe IP with 64-bit addressing, addressing larger than 4GB window and in Root complex mode?
    I need to keep resource of FPGA for other tasks too.