Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Initial Startup
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 356 subscribers
  • Views 2781 views
  • Users 0 members are here
Related

Initial Startup

electrodev99
electrodev99 over 9 years ago

Hello all,

I purchased a MIni-ITX recently, and I guess it was just the FPGA board alone not realzing I needed a power supply and everything else. So I rigged up an ATX Power Cable that has 12V, 5V, and 3.3V coming off of it. This is actually better because I can use my own power supply that I can monitor the power usage on.

Anyway, it didn't come with a SD Card, and it also seems that the SPI Flash was empty too -- so I have been trying to get everything up and running. I attempted to program the QSPI flash with one of the reference designs packages that are included on this website.

I can program the QSPI flash with reference designs and they are verified to be flashing correctly. I also put the Wind River linux on the SD card so that should be correct as well.

Problems:

I am able to program the system over JTAG, but I have to use Vivado 2016.3 so a lot of the material and reference designs are made for older versions. I cannot seem to get Linux or anything to boot up on the system. I also can't seem to have the USB JTAG + USB UART cables connected at the same time. My PC only detects one of them being connected at a time. What could possibly be happening here?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    The Avnet Mini-ITX kit is offered in 3 different configurations:

    1) Board Only Kit (no power supply, cables, or the microSD card). This kit is targeted to high volume customers who would integrate the Mini-ITX board into their system.

    2) Base KIt (includes cables, power supply, and the microSD card).

    3) System Kit (inlcudes the Base Kit + chassis).

     

    It looks like you ordered the Board Only Kit. If included, we ship SanDisk SD/microSD card with all of our Zynq-7000 platforms. Over the past several years, we have noticed this brand of SD/microSD cards work best with the Zynq platforms. I would sugest booting your Mini-ITX board with a Class-10 SanDisk microSD card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • electrodev99
    0 electrodev99 over 9 years ago in reply to e14 Contributor

    Hello npoureh,

    Thank you for the quick response. I can confirm that I ordered the Board Only Kit. I'm assuming it wasn't programmed with the boot code in the QSPI as well.

    Can you help me understand why when I have the USB JTAG connected my USB UART device is no longer detected? If I have the USB UART connected alone it is detected, but once the USB JTAG is connected again it goes away.


    Thanks!
    Matt Griffith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • electrodev99
    0 electrodev99 over 9 years ago in reply to e14 Contributor

    Hello npoureh,

    Thank you for the quick response. I can confirm that I ordered the Board Only Kit. I'm assuming it wasn't programmed with the boot code in the QSPI as well.

    Can you help me understand why when I have the USB JTAG connected my USB UART device is no longer detected? If I have the USB UART connected alone it is detected, but once the USB JTAG is connected again it goes away.


    Thanks!
    Matt Griffith