Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Initial Startup
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 356 subscribers
  • Views 2781 views
  • Users 0 members are here
Related

Initial Startup

electrodev99
electrodev99 over 9 years ago

Hello all,

I purchased a MIni-ITX recently, and I guess it was just the FPGA board alone not realzing I needed a power supply and everything else. So I rigged up an ATX Power Cable that has 12V, 5V, and 3.3V coming off of it. This is actually better because I can use my own power supply that I can monitor the power usage on.

Anyway, it didn't come with a SD Card, and it also seems that the SPI Flash was empty too -- so I have been trying to get everything up and running. I attempted to program the QSPI flash with one of the reference designs packages that are included on this website.

I can program the QSPI flash with reference designs and they are verified to be flashing correctly. I also put the Wind River linux on the SD card so that should be correct as well.

Problems:

I am able to program the system over JTAG, but I have to use Vivado 2016.3 so a lot of the material and reference designs are made for older versions. I cannot seem to get Linux or anything to boot up on the system. I also can't seem to have the USB JTAG + USB UART cables connected at the same time. My PC only detects one of them being connected at a time. What could possibly be happening here?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    At the risk of stating the obvious, the boot mode switch must be set correctly when booting from the SD card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • electrodev99
    0 electrodev99 over 9 years ago in reply to e14 Contributor

    Hello npoureh,

    So I think I figured out the first issue I was having -- I didn't realize it could actually boot everything including programming the FPGA from the SD Card, wow!

    The USB UART vs USB JTAG is probably the last issue -- is it possible to connect both at the same time or not?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to electrodev99

    Not only it is possible, it is vital to be able to connect both USB interfaces during debug/development (we do it all the time).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • electrodev99
    0 electrodev99 over 9 years ago in reply to e14 Contributor

    That is what I figured! Especially when using Xilinx SDK, quick debug + UART printfs. I'm not sure why it immediately kicks off the UART from the Device Manager then. I wasn't sure if this was something you had heard about in problem reports before?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • electrodev99
    0 electrodev99 over 9 years ago in reply to e14 Contributor

    That is what I figured! Especially when using Xilinx SDK, quick debug + UART printfs. I'm not sure why it immediately kicks off the UART from the Device Manager then. I wasn't sure if this was something you had heard about in problem reports before?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to electrodev99

    No, I have not seen this before or aware of any of our customers seeing it.

    Do you have a Xilinx USB-JTAG module you can use for now? Yo can disconnect the JTAG USB cable and connect the Xilinx USB-JTAG moduel to the PC4 header on the Mini-ITX board (J1 next to the U3 JTAG-module).