Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Initial Startup
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 356 subscribers
  • Views 2781 views
  • Users 0 members are here
Related

Initial Startup

electrodev99
electrodev99 over 9 years ago

Hello all,

I purchased a MIni-ITX recently, and I guess it was just the FPGA board alone not realzing I needed a power supply and everything else. So I rigged up an ATX Power Cable that has 12V, 5V, and 3.3V coming off of it. This is actually better because I can use my own power supply that I can monitor the power usage on.

Anyway, it didn't come with a SD Card, and it also seems that the SPI Flash was empty too -- so I have been trying to get everything up and running. I attempted to program the QSPI flash with one of the reference designs packages that are included on this website.

I can program the QSPI flash with reference designs and they are verified to be flashing correctly. I also put the Wind River linux on the SD card so that should be correct as well.

Problems:

I am able to program the system over JTAG, but I have to use Vivado 2016.3 so a lot of the material and reference designs are made for older versions. I cannot seem to get Linux or anything to boot up on the system. I also can't seem to have the USB JTAG + USB UART cables connected at the same time. My PC only detects one of them being connected at a time. What could possibly be happening here?

  • Sign in to reply
  • Cancel
Parents
  • electrodev99
    0 electrodev99 over 9 years ago

    Hello all,

    Turns out both things were user error. Sorry about that! I replaced the micro usb cable I was using and it worked fine.

    Best Regards!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • electrodev99
    0 electrodev99 over 9 years ago

    Hello all,

    Turns out both things were user error. Sorry about that! I replaced the micro usb cable I was using and it worked fine.

    Best Regards!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • electrodev99
    0 electrodev99 over 9 years ago in reply to electrodev99

    I also wanted to mention that you definitely want to have a Class 10 micro SD Card. I had problems with other micro SD Cards (Like a "Strontium" 8Gb card.