Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Mini-ITX self-test - PL DDR issue?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 355 subscribers
  • Views 1481 views
  • Users 0 members are here
Related

Mini-ITX self-test - PL DDR issue?

e14 Contributor
e14 Contributor over 10 years ago

Hello everyone,

Just wondering whether there's a self-test boot image available for the 7045 mini-ITX board. I'm seeing some odd behaviour (more below) which I'm 99% sure it just a configuration/software error but I'd like to be completely eliminate the hardware as a cause. I've found the Out-Of-Box design, but that's only a very basic test (essentially checks that the PS starts up).

 

The problem I'm having: I can only access 512MB of the PL DDR3 RAM. It's mapped into address range 0x8000_0000 to 0xBFFF_FFFF (ie 1GB address space) but everything from 0xA000_0000 to 0xBFFF_FFFF is the same as 0x8000_0000 to 0x9FFF_FFFF. If I write to 0x8000_0000, the same data appears at 0xA000_0000 and vice versa.

Software in use is Vivado 2016.1, Petalinux 2015.4, and a heavily-modified version of the Zynq 7045 Mini-ITX 2015.2.1 Petalinux reference design (I cut out almost all the original hardware blocks to put my own in, but I haven't touched the MIG).

 

Any ideas?

 

Thanks,

Evan

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Evan,

      If you just want to validatate that all the memory is available in bare metal, the SDK can generate a memory test program.  By default, it only tests a portion of available memory (for a quick and speedy check that things are working), but you can easily modify the source to validate the entire available memory.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Evan,

      If you just want to validatate that all the memory is available in bare metal, the SDK can generate a memory test program.  By default, it only tests a portion of available memory (for a quick and speedy check that things are working), but you can easily modify the source to validate the entire available memory.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Ron,

     

    Thanks very much for the reply. I didn't know about that feature in the SDK; it'll definitely be useful. I've done a bit of software-level testing using peek/poke from Petalinux and that is definitely not able to access the upper 512MB of PL RAM.

     

    The problem I have is that I suspect there's actually a problem below the software level, either in the physical hardware (unlikely) or in the bitstream (more likely). What I was hoping to get was a "known-good" self-test bitstream which would distinguish between those scenarios; if a known-good bitstream that works on other mini-ITX boards works fine here then the hardware is fine and somehow Vivado is getting the bitstream generation messed-up; if it fails here then there must be a hardware issue with the board and we should look into replacing it.

    It looks like I can take the Petalinux reference design (which includes a pre-built bitstream) and use that with the SDK, so I'll give that a shot.

     

    Cheers,

    Evan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Ron,

     

    I just gave that a shot, and the PL memory appears to fail. I've tested using the 2015.2 and 2014.2 Petalinux reference designs with the same results. A hardware problem with the board is now looking more likely. Thanks very much for your help.

     

    Cheers,

    Evan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Hello,

    May be it's not really relevant you your subject, but my question is about MIG, PS and PL parts.

    I found some post that the only way to interface DDR is thought PS (since it has an integrated DDR controller) for Zedboard. Is this true for Mini-ITX as well? Is this correct for all Zynq devices? or only for Zedboard?

    What would actually happen if I create only a 'PL' project with MIG IP, since it's providing this option? Moreover it provides an option to have both PS with DDR3 access and a MIG generation as well with it's own DDR controller. Or am I missing something?

    Thank you in advance.