Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Mini-ITX self-test - PL DDR issue?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 355 subscribers
  • Views 1481 views
  • Users 0 members are here
Related

Mini-ITX self-test - PL DDR issue?

e14 Contributor
e14 Contributor over 10 years ago

Hello everyone,

Just wondering whether there's a self-test boot image available for the 7045 mini-ITX board. I'm seeing some odd behaviour (more below) which I'm 99% sure it just a configuration/software error but I'd like to be completely eliminate the hardware as a cause. I've found the Out-Of-Box design, but that's only a very basic test (essentially checks that the PS starts up).

 

The problem I'm having: I can only access 512MB of the PL DDR3 RAM. It's mapped into address range 0x8000_0000 to 0xBFFF_FFFF (ie 1GB address space) but everything from 0xA000_0000 to 0xBFFF_FFFF is the same as 0x8000_0000 to 0x9FFF_FFFF. If I write to 0x8000_0000, the same data appears at 0xA000_0000 and vice versa.

Software in use is Vivado 2016.1, Petalinux 2015.4, and a heavily-modified version of the Zynq 7045 Mini-ITX 2015.2.1 Petalinux reference design (I cut out almost all the original hardware blocks to put my own in, but I haven't touched the MIG).

 

Any ideas?

 

Thanks,

Evan

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Maxxx54,

    It depends on the Zynq board you are looking at. For instance if you look at the Mini-ITX hardware user guide http://zedboard.org/support/documentation/2056 page 14, it states that the Mini-ITX development board utilizes two 1Gb banks of DDR3 memory. One bank resides on the PS side of the Zynq-7000 AP Soc(like ZedBoard), and the other on the PL side. The PL bank pin out is generated by MIG.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Maxxx54,

    It depends on the Zynq board you are looking at. For instance if you look at the Mini-ITX hardware user guide http://zedboard.org/support/documentation/2056 page 14, it states that the Mini-ITX development board utilizes two 1Gb banks of DDR3 memory. One bank resides on the PS side of the Zynq-7000 AP Soc(like ZedBoard), and the other on the PL side. The PL bank pin out is generated by MIG.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Thank, Josh for reply!

    A few more aspects:
    1) Since on Zedboard DDR is only connected to PS side, this would be the only way to access it then (using integrated to PS controller). However it's still possible to insert say MIG controller to Zedboard'd vivado design, although I'm not sure how it'll then handle it further on in implementation parts.. 
    BTW,  since any DDR  controller would need a processing power (either ARM or say a Microblaze) would it be possible to connect MIG controller to ARM core? Or since in Zedboard MIG is not connected with DDR, there is not much use of such an experiments?


    2) Another question is more related to mini-ITX type boards, where 1G DDR is indeed split between PS and PL parts. In such a board I assume it would be possible to use both  MIG (with say Microblaze) and PS parts,  both would need to address different parts of DDR, but still be in the same design. Is it not? Then  it's also should be possible to use ARM to control MIG for DDR access? Question here is also regarding performance, if say I need to transfer data from ADC to DDR (in mini-ITX), which way would be more preferable using pure PS side or MIG + Microblaze or may be ARM and MIG?


    Thank you in advance.