Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZed Petalinux 2010.1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 359 subscribers
  • Views 2933 views
  • Users 0 members are here
Related

MiniZed Petalinux 2010.1

bigguiness
bigguiness over 5 years ago

Hello all,

 

I'm following this, Minized getting started 2020.1 + PYNQ setup , to try and figure out the Petalinux 2010.1 workflow with a MiniZed board.

 

During the "Building project..." stage I got a WARNING and ERROR about speexdsp-1.2rc3-r0 not being found.

 

After quite a while (where I assume it was building the packages) I got this:

 

NOTE: Tasks Summary: Attempted 4686 tasks of which 3322 didn't need to be rerun and all succeeded.

 

Summary: There was 1 WARNING message shown.

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

ERROR: Failed to build avnet-image-full

 

It's still building but I was wondering how I can fix the WARNING/ERROR and how do you do a rebuild without going through the initial part that builds seems to build the Vivado part?

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • bhfletcher
    bhfletcher over 5 years ago in reply to bigguiness +1
    That ( 2020p1_minized_20201104_065342 ) is not the correct tag. Please try refreshing your checkout. I think you may have pulled a preliminary version. You can see the correct tags documented in this blog…
Parents
  • bigguiness
    bigguiness over 5 years ago

    Well.. the build appears to be stuck here:

     

    NOTE: Resolving any missing task queue dependencies

    Initialising tasks: 100% |###################################################################################################################################################################################| Time: 0:00:18

    Checking sstate mirror object availability: 100% |###########################################################################################################################################################| Time: 0:00:33

    Sstate summary: Wanted 210 Found 25 Missed 185 Current 1179 (11% match, 86% complete)

    NOTE: Executing Tasks

    NOTE: Setscene tasks completed

    Currently  1 running tasks (4166 of 4645)  89% |#########################################################################################################################################################                  |

    0: linux-xlnx-5.4+gitAUTOINC+22b71b4162-r0 do_compile - 2h12m31s (pid 9082)

     

    It's been at 89% for about an hour. I'm leaving it running for now to see if it ever finishes.

     

    Any ideas...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 5 years ago in reply to bigguiness

    It appears the build task it is stuck is on compiling the kernel.  Depending on your PC resources (RAM, CPU cores, etc.) it can take a long time to complete some build tasks like compiling the kernel.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • narrucmot
    narrucmot over 5 years ago in reply to bigguiness

    It appears the build task it is stuck is on compiling the kernel.  Depending on your PC resources (RAM, CPU cores, etc.) it can take a long time to complete some build tasks like compiling the kernel.

     

    --Tom