Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZed Petalinux 2010.1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 359 subscribers
  • Views 2933 views
  • Users 0 members are here
Related

MiniZed Petalinux 2010.1

bigguiness
bigguiness over 5 years ago

Hello all,

 

I'm following this, Minized getting started 2020.1 + PYNQ setup , to try and figure out the Petalinux 2010.1 workflow with a MiniZed board.

 

During the "Building project..." stage I got a WARNING and ERROR about speexdsp-1.2rc3-r0 not being found.

 

After quite a while (where I assume it was building the packages) I got this:

 

NOTE: Tasks Summary: Attempted 4686 tasks of which 3322 didn't need to be rerun and all succeeded.

 

Summary: There was 1 WARNING message shown.

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

ERROR: Failed to build avnet-image-full

 

It's still building but I was wondering how I can fix the WARNING/ERROR and how do you do a rebuild without going through the initial part that builds seems to build the Vivado part?

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • bhfletcher
    bhfletcher over 5 years ago in reply to bigguiness +1
    That ( 2020p1_minized_20201104_065342 ) is not the correct tag. Please try refreshing your checkout. I think you may have pulled a preliminary version. You can see the correct tags documented in this blog…
Parents
  • narrucmot
    narrucmot over 5 years ago

    Hi Hartley,

     

    You are correct that the MiniZed BSP build script also builds the underlying hw platform in Vivado.  The build script senses if the hw project has been built and runs Vivado in the background to build it.  This also means that the hw project only has to be built once.  The next time the BSP build script is run it will just grab the Vivado xsa and bitstream files and import them into the PetaLinux project.  This saves significant time.

     

    A PetaLinux build requires an active internet connection, and the "ERROR about speexdsp-1.2rc3-r0 not being found" error you mention could be the result of a few things:

    • Your internet connection having problems
    • The server where the speexdsp package is hosted is having internet connection problems
    • The speexdsp package files have moved to a different server, or the version has changed, but the package build recipe has not be updated

     

    Sometimes this warning/error will fix itself on a retry of the build.  Quite often this error will fix itself (e.g. the package recipe will find alternate hosting sites for the package sources) while the BSP is being built. 

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bigguiness
    bigguiness over 5 years ago in reply to narrucmot

    Should I just kill the build and run the ./make_minized.sh script again?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 5 years ago in reply to bigguiness

    Killing the PetaLinux build is sometimes tricky.  It does not like to be killed and will often hang.  If you do that you should reboot to be sure there aren't any stray processes still running.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bigguiness
    bigguiness over 5 years ago in reply to narrucmot

    Hmmm. A Ctrl-C didn't kill the build. It appears to have restarted it.

     

    Looking at the log it looks like it has restarted a couple times. Is this normal?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bigguiness
    bigguiness over 5 years ago in reply to bigguiness

    The ./make_minized.sh script finally finished but I did a Ctrl+C a number of times when it appeared to hang while compiling the kernel. Not sure what effect that will have.

     

    I think running the script again and just letting it try to finish overnight may be worthwhile. What is the best way to ensure that the build is clean?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 5 years ago in reply to bigguiness

    The best way to do a clean and rebuild is the following concatenated (&&) commands:

    $ petalinux-build -x mrproper --force && petalinux-build

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • narrucmot
    narrucmot over 5 years ago in reply to bigguiness

    The best way to do a clean and rebuild is the following concatenated (&&) commands:

    $ petalinux-build -x mrproper --force && petalinux-build