Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZed PDM reference design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1034 views
  • Users 0 members are here
Related

MiniZed PDM reference design

kchp
kchp over 8 years ago
Hello,
I am currently going through the reference design for using the onboard microphone, but have run into a bit of an issue with the PreLoadFcn for the Simulink model.
When I open the model I am presented with a diagnostics window with a warning
 
Index in position 2 exceeds array bounds (must not exceed 1).
 
This issue seems to prevent me from running the simulation as the ila_data_struct isn't created. Has anyone else encountered this issue and found a solution. Or is it possible to skib this part and go straight to the next section?
 
I am running this with System Generator 2018.2 and Matlab R2018a.
 
  • Sign in to reply
  • Cancel
  • stefanrousseau
    0 stefanrousseau over 8 years ago

    Hello,

    Are you able to run the TCL script that generates the Vivado design without problems, or does it give you errors at that stage?

    Thanks,

    Stefan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kchp
    0 kchp over 8 years ago

    Hello Stefan,

    No, I'm not able to run the TCL script to completion. So far I have encountered two errors, the first was a version check so worked around this be setting 'version_override=yes'
    The error I'm currently stuck on gives the error message:

    ERROR: [Board 49-71] The board_part definition was not found for em.avnet.com:minized:part0:1.2. The project's board_part property was not set, but the project's part property was set to xc7z007sclg225-1. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command. Check if board.repoPaths parameter is set and the board_part is installed from the tcl app store.

    Thanks

     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • stefanrousseau
    0 stefanrousseau over 8 years ago

    Overriding the tools version check is fine, as this build does work current tools versions (at the time that the script was generated, this could of course not be predicted).  But to use MiniZed, you first have to exit Vivado, instal the board definition files in the Vivado tools directory, and then start Vivado again.  Please see: "Board Definition Files" on minized.org/product/minized under "Documentation.

    Regards,
    Stefan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • kchp
    0 kchp over 8 years ago in reply to stefanrousseau

    Cheers Stefan
    That got the TCL script to complete.