Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZed PDM reference design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1036 views
  • Users 0 members are here
Related

MiniZed PDM reference design

kchp
kchp over 8 years ago
Hello,
I am currently going through the reference design for using the onboard microphone, but have run into a bit of an issue with the PreLoadFcn for the Simulink model.
When I open the model I am presented with a diagnostics window with a warning
 
Index in position 2 exceeds array bounds (must not exceed 1).
 
This issue seems to prevent me from running the simulation as the ila_data_struct isn't created. Has anyone else encountered this issue and found a solution. Or is it possible to skib this part and go straight to the next section?
 
I am running this with System Generator 2018.2 and Matlab R2018a.
 
  • Sign in to reply
  • Cancel
Parents
  • kchp
    0 kchp over 8 years ago

    Hello Stefan,

    No, I'm not able to run the TCL script to completion. So far I have encountered two errors, the first was a version check so worked around this be setting 'version_override=yes'
    The error I'm currently stuck on gives the error message:

    ERROR: [Board 49-71] The board_part definition was not found for em.avnet.com:minized:part0:1.2. The project's board_part property was not set, but the project's part property was set to xc7z007sclg225-1. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command. Check if board.repoPaths parameter is set and the board_part is installed from the tcl app store.

    Thanks

     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kchp
    0 kchp over 8 years ago

    Hello Stefan,

    No, I'm not able to run the TCL script to completion. So far I have encountered two errors, the first was a version check so worked around this be setting 'version_override=yes'
    The error I'm currently stuck on gives the error message:

    ERROR: [Board 49-71] The board_part definition was not found for em.avnet.com:minized:part0:1.2. The project's board_part property was not set, but the project's part property was set to xc7z007sclg225-1. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command. Check if board.repoPaths parameter is set and the board_part is installed from the tcl app store.

    Thanks