Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZed board not detected by Vivado/SDK
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1520 views
  • Users 0 members are here
Related

MiniZed board not detected by Vivado/SDK

marandil
marandil over 8 years ago

Hello, I am currently experiencing a following issue:

I'm trying to get my MiniZed board started using Linux (more precisely a personalized version of LMDE, mostly compatible with Ubuntu). When I connect the board using a USB cable, it's properly detected by the operating system:

[  139.563349] usb 3-2: new high-speed USB device number 7 using xhci_hcd
[  139.707309] usb 3-2: New USB device found, idVendor=0403, idProduct=6010
[  139.707322] usb 3-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[  139.707323] usb 3-2: Product: JTAG+Serial
[  139.707324] usb 3-2: Manufacturer: Xilinx
[  139.707325] usb 3-2: SerialNumber: 1234-oj1
[  139.709214] ftdi_sio 3-2:1.0: FTDI USB Serial Device converter detected
[  139.709260] usb 3-2: Detected FT2232H
[  139.709489] usb 3-2: FTDI USB Serial Device converter now attached to ttyUSB0
[  139.710870] ftdi_sio 3-2:1.1: FTDI USB Serial Device converter detected
[  139.710902] usb 3-2: Detected FT2232H
[  139.711038] usb 3-2: FTDI USB Serial Device converter now attached to ttyUSB1

Using `screen /dev/ttyUSB1 115200` I can successfully communicate with the pre-installed PetaLinux. I can't, however, use Vivado or Xilinx SDK to program/debug, even a simple code.

I tried following the MiniZed tutorials and basically stopped at the same point as mentioned in http://www.zedboard.org/content/sdk-cant-program-fpga-minized, which is the "Program FPGA" step.

I was successful in getting past that point on the same machine, but using Windows (which is NOT my preferred solution). I have checked the BSP settings in the Xilinx SDK and they seem consistent between operating systems.

Is there any additional guide how to setup the hardware server properly to use the board under Linux? I assume that the (Xilinx) Hardware Manager does not know that the JTAG is present at /dev/ttyUSB0.

For the record, I have imported the MiniZed board package and I'm running Vivado 2017.4.

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Try downloading and installing the FTDI Driver on your machine.

    Please see page 11 step 4 in the getting started guide. http://zedboard.org/sites/default/files/documentations/MiniZed-GSG-v1_1.pdf

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • marandil
    0 marandil over 8 years ago in reply to jafoste4

    Hi

    Thanks for the advice, but VCP FTDI drivers are built-in into Linux kernel, which I confirmed already.

    $ lsmod | grep ftdi
    ftdi_sio 53248 0
    usbserial 49152 1 ftdi_sio
    usbcore 249856 9 uvcvideo,usbhid,ehci_hcd,ftdi_sio,usbserial,xhci_pci,btusb,xhci_hcd,ehci_pci

    The presence of the drivers in the kernel is also mentioned on the FTDI page linked in the GSG.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    You may want to check out the : Development Using Ubuntu Desktop Linux

    guide located here http://zedboard.org/support/design/18891/146
     
    --Josh
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • marandil
    0 marandil over 8 years ago in reply to jafoste4

    Thanks for the tip.

    I found the solution in one of the linked guides, but I must say that the titles are quite misleading ("VirtualBox and Linux VM Installation Guide v2017.2" and "OracleRegistered VM VirtualBox Installation Instructions for Windows 7 and Linux Virtual Machine Creation Targeting Avnet Development Boards").

    For reference, the solution was to install additional Xilinx drivers:

    # cd /opt/Xilinx/Vivado/2017.?/data/xicom/cable_drivers/lin64/install_script/install_drivers/
    # ./install_drivers

    Cheers!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer