Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design AXI Transer between linux and FPGA
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 359 subscribers
  • Views 1291 views
  • Users 0 members are here
Related

AXI Transer between linux and FPGA

shanbhagm
shanbhagm over 8 years ago

Hi,

My requirement is to transfer data from FPGA to ARM(linux) and back. I want to use the AXI bus interface.

Can some one point me to aworking example of data transfer from linux to the FPGA and vise versa.

A quick help will be appreciable.

-Madhav

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    My suggestion would be for you to take the free Integrating Sensors on MiniZed with Petalinux Speedway we offer. It can be found here

    http://zedboard.org/support/trainings-and-videos

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    My suggestion would be for you to take the free Integrating Sensors on MiniZed with Petalinux Speedway we offer. It can be found here

    http://zedboard.org/support/trainings-and-videos

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shanbhagm
    0 shanbhagm over 8 years ago in reply to jafoste4
    Hi,
     
    I have followed the step with Xilinx_Vivado_SDK_Web_2018.2_0614_1954_Lin64.bin and petalinux-v2018.2-final-installer.run.
     
    When I try to build peta linux I get the following error in Lab1 .
     
    Can you help me on same.
     
      training@training-VirtualBox:~/labs/lab1/petalinux-min$ petalinux-config  --get-hw-description=~/hdl/Projects/minized_sensor_fusion/MINIZED/minized_sensor_fusion.sdk
      INFO: Getting hardware description...
      INFO: Rename minized_sensor_fusion_hw.hdf to system.hdf
      [INFO] generating Kconfig for project
                                                                                      
      [INFO] menuconfig project
      /home/training/labs/lab1/petalinux-min/build/misc/config/Kconfig.syshw:30:warning: defaults for choice values not supported
      /home/training/labs/lab1/petalinux-min/build/misc/config/Kconfig:597:warning: config symbol defined without type
       
       
      *** End of the configuration.
      *** Execute 'make' to start the build or try 'make help'.
       
      [INFO] sourcing bitbake
      [INFO] generating plnxtool conf
      [INFO] generating meta-plnx-generated layer
      [INFO] generating machine configuration
      [INFO] generating bbappends for project . This may take time ! 
      [INFO] generating u-boot configuration files
                                                                                                                                                                    
      [INFO] generating kernel configuration files
      [INFO] generating kconfig for Rootfs
      [INFO] oldconfig rootfs
      [INFO] generating petalinux-user-image.bb
      training@training-VirtualBox:~/labs/lab1/petalinux-min$ petalinux-build 
      [INFO] building project
      [INFO] sourcing bitbake
      INFO: bitbake petalinux-user-image
      Parsing recipes: 100% |########################################################################################################################| Time: 0:01:22
      Parsing of 2552 .bb files complete (0 cached, 2552 parsed). 3425 targets, 148 skipped, 0 masked, 0 errors.
      WARNING: No recipes available for:
        /home/training/labs/lab1/petalinux-min/project-spec/meta-plnx-generated/recipes-bsp/device-tree/device-tree-generation_%.bbappend
        /home/training/labs/lab1/petalinux-min/project-spec/meta-user/recipes-bsp/device-tree/device-tree-generation_%.bbappend
      NOTE: Resolving any missing task queue dependencies
      Initialising tasks: 100% |#####################################################################################################################| Time: 0:00:09
      Checking sstate mirror object availability: 100% |#############################################################################################| Time: 0:00:18
      NOTE: Executing SetScene Tasks
      NOTE: Executing RunQueue Tasks
      ERROR: device-tree-xilinx+gitAUTOINC+f38738e568-r0 do_compile: Function failed: do_compile (log file is located at /home/training/labs/lab1/petalinux-min/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/device-tree/xilinx+gitAUTOINC+f38738e568-r0/temp/log.do_compile.11307)
      ERROR: Logfile of failure stored in: /home/training/labs/lab1/petalinux-min/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/device-tree/xilinx+gitAUTOINC+f38738e568-r0/temp/log.do_compile.11307
      Log data follows:
      | DEBUG: Executing shell function do_compile
      | /home/training/labs/lab1/petalinux-min/build/../components/plnx_workspace/device-tree/device-tree/system-top.dts:34:28: fatal error: system-user.dtsi: No such file or directory
      | compilation terminated.
      | WARNING: /home/training/labs/lab1/petalinux-min/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/device-tree/xilinx+gitAUTOINC+f38738e568-r0/temp/run.do_compile.11307:1 exit 1 from 'gcc -E -nostdinc -Ulinux -x assembler-with-cpp -I/home/training/labs/lab1/petalinux-min/build/../components/plnx_workspace/device-tree/device-tree -I/home/training/labs/lab1/petalinux-min/build/tmp/work-shared/plnx-zynq7/kernel-source/include -I/home/training/labs/lab1/petalinux-min/build/tmp/work-shared/plnx-zynq7/kernel-source/include -I/home/training/labs/lab1/petalinux-min/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/device-tree/xilinx+gitAUTOINC+f38738e568-r0 -o `basename ${DTS_FILE}`.pp ${DTS_FILE}'
      | ERROR: Function failed: do_compile (log file is located at /home/training/labs/lab1/petalinux-min/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/device-tree/xilinx+gitAUTOINC+f38738e568-r0/temp/log.do_compile.11307)
      ERROR: Task (/opt/pkg/petalinux/components/yocto/source/arm/layers/meta-xilinx/meta-xilinx-bsp/recipes-bsp/device-tree/device-tree.bb:do_compile) failed with exit code '1'
      NOTE: Tasks Summary: Attempted 2970 tasks of which 2847 didn't need to be rerun and 1 failed.
       
      Summary: 1 task failed:
        /opt/pkg/petalinux/components/yocto/source/arm/layers/meta-xilinx/meta-xilinx-bsp/recipes-bsp/device-tree/device-tree.bb:do_compile
      Summary: There was 1 WARNING message shown.
      Summary: There was 1 ERROR message shown, returning a non-zero exit code.
      ERROR: Failed to build project