Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Simulink led blinking External mode issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 898 views
  • Users 0 members are here
Related

Simulink led blinking External mode issue

100stefanoo
100stefanoo over 8 years ago

sorry to bother, my misfortune with this project is neverending... still trying to run the Simulink led_blinking_4bit example.

HDL workflow was successful, the led on the board is blinking properly and I have the Software Interface Model open. Then when I try to proceed for External Mode I cannot press "Run" but only "Connect to Target" and i get this error:

The model is not configured for External mode.

My Support packages result all up to date, I can ping the board which is connected thru WiFi.

Simulink 2017b
Vivado 2017.2
Embedded coder Xilinx 17.2.1
 

  • Sign in to reply
  • Cancel

Top Replies

  • 100stefanoo
    100stefanoo over 8 years ago +1 verified
    Problem solved installing "Simulink Coder", my fault I was confident to have it simply because I used to have it in the past... now the demo works as expected and no need to change wireless card or to…
Parents
  • 100stefanoo
    0 100stefanoo over 8 years ago

    Problem solved installing "Simulink Coder", my fault I was confident to have it simply because I used to have it in the past... now the demo works as expected and no need to change wireless card or to setenv the IP.

    I realized that when trying to deploy an older project to Arduino, the diagnostic error message was much more clear stating "you don't have Simulink Coder" instead of " model not configured for External mode".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • 100stefanoo
    0 100stefanoo over 8 years ago

    Problem solved installing "Simulink Coder", my fault I was confident to have it simply because I used to have it in the past... now the demo works as expected and no need to change wireless card or to setenv the IP.

    I realized that when trying to deploy an older project to Arduino, the diagnostic error message was much more clear stating "you don't have Simulink Coder" instead of " model not configured for External mode".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • mbrown
    0 mbrown over 8 years ago in reply to 100stefanoo

    Thanks for responding with the solution. The error message should be improved for the Zynq flow.

    /Matt