Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZed Development Process Help
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 1693 views
  • Users 0 members are here
  • petalinux
  • minized
Related

MiniZed Development Process Help

dlux
dlux over 7 years ago

Hello,

 

I would like some help determining the development process for the MiniZed. Essentially, I am trying to create my own custom verilog code as well as C code, while still having petalinux and WiFi functionality. Currently I am trying my best to follow the "Integrating Sensors on MiniZed with PetaLinux (2017.1 and 2017.4)" tutorial. My problem with this tutorial is that too many of the files are pre-generated. Specifically, LAB1 shows how to create a boot.bin file for QSPI programming and then LAB2 shows how to program the image.ub into the emmc, but it also includes a bootemmc.bin file. As far as I understand, the bootemmc.bin file is also reprogramming the QSPI flash. Is there is difference between boot.bin of LAB1 and bootemmc.bin of LAB2? Maybe I am missing something, but I cannot seem to find how to generate the bootemmc.bin file. How is this possible?

 

I would like to generate a base project where I can develop my own PL and PS code. What I have tried so far:

 

1. Generate a project using petalinux-create using the bsp "MiniZed.bsp 2018.2 (BSP for booting from QSPI flash to eMMC)"

2. When I open the Vivado project created by this command the following files are missing:

     a) wireless_mgr.vhd

     b) minized_LEDs.xdc

     c) bitstream_compression_enable.xdc

     d) minized_petalinux.xdc

3. I found these missing files at https://github.com/Avnet/hdl and inserted them where Vivado was looking for them. Why is this necessary or how do I handle this properly?

4. Bit stream in Vivado was then successfully generated. Now I know I could edit the hardware design and it would successfully generate the bit and hdf files.

5. Exported the necessary HDF from Vivado and ran petalinux-config using the newly generated .hdf file

6. Exited the "Xilinx PetaLinux configuration editor" without changing anything

7. Ran petalinux-build

8. Now this is where some confusion comes into play:

     a) the petalinux-build command generated a boot.bin file without running boot_gen.sh! So, I tried programming this boot.bin file using "exec program_flash -f boot.bin -fsbl zynq_fsbl.elf -flash_type qspi_single" (on Windows). The "zynq_fsbl.elf" was also taken from the generated files from petalinux-build. This messed up the system enough that I got error "Zynq> ERROR: [Xicom 50-186] Error while detecting SPI flash device - unrecognized JEDEC id bytes: 00, 00, 00" when trying to follow "Restoring MiniZed to the Factory State" using XSCT (on Windows). I had to use the "Programming the QSPI Flash from the Vivado Hardware Manager" section of that file to get it back to normal (again on Windows).

     b) I adapted the boot_gen.sh script to work with my project. I thought maybe the starting addresses were incorrect in the boot.bin file generated purely from petalinux-build. In this case when using the Vivado Hardware Manager on Windows to program the flash using this boot.bit file, I get the error. "ERROR: [Labtools 27-3347] Flash Programming Unsuccessful: Program File Size cannot be greater than flash part size".

     c) I have not tried using petalinux-package as this was not used in any of Avnet's documentation (besides generating BSPs, from what I've seen).

 

This is my current attempt and thought process. I will follow LAB6 of "Integrating Sensors on MiniZed with PetaLinux (2017.1 and 2017.4)" to add my own C application, once I get there. For now, I want to to be able to generate the bootemmc.bin and image.ub files for a QSPI and eMMC build using the "MiniZed.bsp 2018.2 (BSP for booting from QSPI flash to eMMC)" as a basis. I am unsure if I am going about this correctly. Feel free to give me any suggestions and pointers you seem necessary.

 

Furthermore, running any of the MiniZed scripts at https://github.com/Avnet/hdl does nothing on both Windows and linux.

 

I am running Vivado 2018.2 on WIndows 10

I used the prebuilt virtual box image file for Ubuntu 16.04. I had to update some files to properly run Vivado/SDK 2018.2. I also installed petalinux 2018.2 tools.

 

Thanks for your help,

Richard

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 7 years ago +1
    I can't help you with specifics, but I found the following to be great resources when getting to grips with the Zynq. The Avnet Speedway Workshops are pretty much the same as the Path to Programmable challenge…
Parents
  • jafoste4
    0 jafoste4 over 7 years ago

    Hi Richard,

    UG1144 is always a good place to get started when learning PetaLinux development.

     

    https://www.xilinx.com/support/documentation/sw_manuals/xilinx2018_2/ug1144-petalinux-tools-reference-guide.pdf

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 7 years ago

    Hi Richard,

    UG1144 is always a good place to get started when learning PetaLinux development.

     

    https://www.xilinx.com/support/documentation/sw_manuals/xilinx2018_2/ug1144-petalinux-tools-reference-guide.pdf

     

    -Josh