Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZED Vivado VM image ?   the document really does not spell out where this VM image is ?  Any help ?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 8 answers
  • Subscribers 361 subscribers
  • Views 3612 views
  • Users 0 members are here
Related

MiniZED Vivado VM image ?   the document really does not spell out where this VM image is ?  Any help ?

gregcasey
gregcasey over 6 years ago

The MiniZED makes a special point of having you install the Oracle Virtual Box  -- got that all done.   Then it says there is a pre-loaded image for Vivado?   Where is it?  

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 6 years ago +2 suggested
    There are quite a few broken links and URLs in the guide. There's also quite a few places where it still mentions version 2017.4 (I think). I found that installing Vivado and SDK/Vitis directly on a Windows…
  • gregcasey
    gregcasey over 6 years ago +2
    Ok, loaded Vitis. I think I am moving ahead, but very slowly to do a Hello World Lab it is unfortunate that the initial training has some many issues without clarity. My humble feedback at this point,…
  • Fred27
    Fred27 over 6 years ago +1 suggested
    I managed to follow both the HW and SW tutorials using Vivado installed directly on Windows 10. No need for a VM. I managed to use 2019.2 and Vitis without too much trouble - the main different is how…
Parents
  • Fred27
    0 Fred27 over 6 years ago

    I managed to follow both the HW and SW tutorials using Vivado installed directly on Windows 10. No need for a VM.

     

    I managed to use 2019.2 and Vitis without too much trouble - the main different is how a project and BSP is started in Vitis compared to the SDK in 2019.1. I'm not sure exactly where in the labs you are, but if you've installed 2019.2 too then I suspect you might be at this point.

     

    The lab is probably expecting you to be running the SDK. You'll need to run Vitis, pick a workspace and "Create Application Project" and then create a new platform for hardware (XSA). To be honest it's a little too much to explain in a single post. You might find it useful to follow a guide that uses Vitis first such as https://www.hackster.io/adam-taylor/mini-but-mighty-the-minized-and-vitis-for-motor-control-9c376b

     

    I've just moved on the Petalinux stuff and trying to use 2019.2 which is confusing the hell out of me (again).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Fred27
    0 Fred27 over 6 years ago

    I managed to follow both the HW and SW tutorials using Vivado installed directly on Windows 10. No need for a VM.

     

    I managed to use 2019.2 and Vitis without too much trouble - the main different is how a project and BSP is started in Vitis compared to the SDK in 2019.1. I'm not sure exactly where in the labs you are, but if you've installed 2019.2 too then I suspect you might be at this point.

     

    The lab is probably expecting you to be running the SDK. You'll need to run Vitis, pick a workspace and "Create Application Project" and then create a new platform for hardware (XSA). To be honest it's a little too much to explain in a single post. You might find it useful to follow a guide that uses Vitis first such as https://www.hackster.io/adam-taylor/mini-but-mighty-the-minized-and-vitis-for-motor-control-9c376b

     

    I've just moved on the Petalinux stuff and trying to use 2019.2 which is confusing the hell out of me (again).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer