Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design MiniZED Vivado VM image ?   the document really does not spell out where this VM image is ?  Any help ?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 8 answers
  • Subscribers 361 subscribers
  • Views 3612 views
  • Users 0 members are here
Related

MiniZED Vivado VM image ?   the document really does not spell out where this VM image is ?  Any help ?

gregcasey
gregcasey over 6 years ago

The MiniZED makes a special point of having you install the Oracle Virtual Box  -- got that all done.   Then it says there is a pre-loaded image for Vivado?   Where is it?  

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 6 years ago +2 suggested
    There are quite a few broken links and URLs in the guide. There's also quite a few places where it still mentions version 2017.4 (I think). I found that installing Vivado and SDK/Vitis directly on a Windows…
  • gregcasey
    gregcasey over 6 years ago +2
    Ok, loaded Vitis. I think I am moving ahead, but very slowly to do a Hello World Lab it is unfortunate that the initial training has some many issues without clarity. My humble feedback at this point,…
  • Fred27
    Fred27 over 6 years ago +1 suggested
    I managed to follow both the HW and SW tutorials using Vivado installed directly on Windows 10. No need for a VM. I managed to use 2019.2 and Vitis without too much trouble - the main different is how…
Parents
  • Fred27
    0 Fred27 over 6 years ago

    There are quite a few broken links and URLs in the guide. There's also quite a few places where it still mentions version 2017.4 (I think).

     

    I found that installing Vivado and SDK/Vitis directly on a Windows 10 machine was fine for following the Hardware and Software courses. No need for the VM. (I was also trying PetaLinux tools installed within WSL2 which initially seems OK, but I'm being bitten by the fact I installed 2019.2 at the moment.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Fred27
    0 Fred27 over 6 years ago

    There are quite a few broken links and URLs in the guide. There's also quite a few places where it still mentions version 2017.4 (I think).

     

    I found that installing Vivado and SDK/Vitis directly on a Windows 10 machine was fine for following the Hardware and Software courses. No need for the VM. (I was also trying PetaLinux tools installed within WSL2 which initially seems OK, but I'm being bitten by the fact I installed 2019.2 at the moment.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ralphjy
    0 ralphjy over 6 years ago in reply to Fred27

    In my brief experience with the Xilinx tools I've decided to take the path most traveled (which I think is Linux).  I'm glad that you've got things working on Windows and I'll be interested hearing about your progress.  I have a dedicated Linux box but I've gone the VM on Windows route because of all the different dependencies between the tool versions and OS versions and also because it seems like this path is pretty well supported by Xilinx and Avnet .  I have different VMs for each combination that I use.  I have learned to be very careful to not update the OS once it is installed.  I hate that minor OS versions cause problems with the tools (e.g. I had problems using Ubuntu 16.04.6 with the 2018.3 tools when I was working with the Ultra96v2.  I had to downgrade to 16.04.4 to get things to work).  I was particularly worried about running PetaLinux with WSL as I haven't used WSL much and Ubuntu in VirtualBox seems to have a lot more mileage on it.  I guess I'm a lot less adventurous in my old age image.  It would be nice if pre-built VM images were available for the different variants that are recommended (maybe the links just need to be fixed?).  External disks are pretty cheap nowadays so I don't mind having having a plethora of VMs - just need a spreadsheet to keep track of what I put in them image. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer