Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Petalinux - MiniZed packages not visible rootfs
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 1767 views
  • Users 0 members are here
  • petalinux
  • minized
Related

Petalinux - MiniZed packages not visible rootfs

bartokon
bartokon over 6 years ago

Hello!

 

I have small problem with visibility of meta-user packages.

 

I have copied all "project-spec/meta-user/*" files from BSP 2019.1 to 2019.2 and I can't see any new fields in "petalinux-config -c rootfs", but if I add contents of "/project-spec/meta-user/recipes-core/images/petalinux-user-image.bb(meta-user copied)" to "/project-spec/meta-plnx-generated/recipes-core/images/petalinux-image.bbappend (meta-plnx-generated autogenerated)" petalinux builds fine. But this is uncomfortable for use and is just bad because it resets after any change to sys-root.

 

The question is how can I make those packages visible in rootfs? There should be new row with userapps, wifi drivers etc. What I'm missing? Avnet speedway workshop miss those details and I couldn't find solution there.

 

Thanks for help!

 

Minized BSP 2019.2 Vitis Ready + WIFI it uses /run/media/mmcblk1p2 as root filesystem (extract whole root image there from tar.gz), put rest of generated petalinux files to /run/media/mmcblk1p1

image

BSP Link

https://drive.googlel.com/open?id=1bOaXwf9CR_OSKg-2gOfmMrGM84EjBUP4

 

Also this BSP can have many, many flaws that I'm unaware of so use it with caution and at your own risk image

  • Sign in to reply
  • Cancel

Top Replies

  • narrucmot
    narrucmot over 6 years ago +1 verified
    Starting with PetaLinux 2019.2 Xilinx made the change that user's custom additions to the <>/ project-spec/meta-user/recipes-core/images/petalinux-user-image.bb file are no longer supported. Apparently…
Parents
  • narrucmot
    0 narrucmot over 6 years ago

    Starting with PetaLinux 2019.2 Xilinx made the change that user's custom additions to the <>/project-spec/meta-user/recipes-core/images/petalinux-user-image.bb file are no longer supported.  Apparently this was some sort of violation of yocto rules to use .bb files for kconfig options.  Instead users must now create a <>/project-spec/meta-user/conf/user-rootfsconfig file with contents that look similar to this:

    #Note: Mention Each package in individual line

    #These packages will get added into rootfs menu entry

     

    CONFIG_gpio-demo

    CONFIG_peekpoke

     

    More information about this change can be found in Appendix A of Xilinx UG1144.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 6 years ago

    Starting with PetaLinux 2019.2 Xilinx made the change that user's custom additions to the <>/project-spec/meta-user/recipes-core/images/petalinux-user-image.bb file are no longer supported.  Apparently this was some sort of violation of yocto rules to use .bb files for kconfig options.  Instead users must now create a <>/project-spec/meta-user/conf/user-rootfsconfig file with contents that look similar to this:

    #Note: Mention Each package in individual line

    #These packages will get added into rootfs menu entry

     

    CONFIG_gpio-demo

    CONFIG_peekpoke

     

    More information about this change can be found in Appendix A of Xilinx UG1144.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • bartokon
    0 bartokon over 6 years ago in reply to narrucmot

    Yes that works, thanks for help!