Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Minized Petalinux 2020 - WiFi Shell Script
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 359 subscribers
  • Views 1336 views
  • Users 0 members are here
  • minized petalinux
  • avnet
  • petalinux2020
Related

Minized Petalinux 2020 - WiFi Shell Script

apadana1984
apadana1984 over 6 years ago

Hello,

 

I am building Petalinux 2020.1 for my Minized Board. I downloaded the Avnet BSP package. I noticed that the default Shell script for enabling the WiFi module has an issue:

 

#Mount the eMMC

echo "Mount the eMMC."

mount /dev/mmcblk1p1 /mnt

 

When I boot my Petalinux, there is not such "mmcblk1p1". There is "mmcblk0p1". What is the best way to correct this file? I changed it and re-built my Petalinux, however, the shell script in the image file didn't change!!! Am I missing something?

 

Also, I changed my "wpa_supplicant.conf" file to include my WiFi user ID&PASSWD, however, the file doesn't change in the linux image file.

 

I appreciate if someone can look into this problem.

 

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • narrucmot
    narrucmot over 6 years ago +1 suggested
    Hi Iman, That shell script (wifi.sh?) has been used for years, so I am surprised that it is breaking now. I will look into this. The reason why the script reverts to its original state on a reboot is because…
Parents
  • narrucmot
    0 narrucmot over 6 years ago

    Hi Iman,

     

    That shell script (wifi.sh?) has been used for years, so I am surprised that it is breaking now.  I will look into this.

     

    The reason why the script reverts to its original state on a reboot is because the MiniZed, by default, boots a RAMdisk root filesystem.  This means the entire filesystem exists in RAM while the system is booted and is thus volatile.  Changes and edits to files are not persistent on a reboot.  That is why the wpa_supplicant.conf file, once edited with your WLAN SSID and password information, is meant to be stored on the FAT partition of the eMMC (mmcblk<0|1>p1) memory.

     

    The MiniZed can be configured to boot the Linux kernel from QSPI and mount a persistent filesystem on a EXT4 partition of the eMMC.  I believe there are shell scripts provided in the BSP that will program the QSPI and eMMC for this boot method.

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 6 years ago

    Hi Iman,

     

    That shell script (wifi.sh?) has been used for years, so I am surprised that it is breaking now.  I will look into this.

     

    The reason why the script reverts to its original state on a reboot is because the MiniZed, by default, boots a RAMdisk root filesystem.  This means the entire filesystem exists in RAM while the system is booted and is thus volatile.  Changes and edits to files are not persistent on a reboot.  That is why the wpa_supplicant.conf file, once edited with your WLAN SSID and password information, is meant to be stored on the FAT partition of the eMMC (mmcblk<0|1>p1) memory.

     

    The MiniZed can be configured to boot the Linux kernel from QSPI and mount a persistent filesystem on a EXT4 partition of the eMMC.  I believe there are shell scripts provided in the BSP that will program the QSPI and eMMC for this boot method.

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • apadana1984
    0 apadana1984 over 6 years ago in reply to narrucmot

    Thank you Tom. By non-updating scripts, I meant the scripts in "rootfs.wic" file created in the host Linux machine. There are two directories in which we can find "rootfs.wic":

     

    1. <project-home>/images/linux/
    2. <project-home>/pre-built/linux/images

     

    The first one updates once we build the Petalinux project. But the second one doesn't update. Maybe its name "pre-built" implies that.(?!)

     

    Iman