Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Minized Petalinux 2020 - WiFi Shell Script
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 359 subscribers
  • Views 1336 views
  • Users 0 members are here
  • minized petalinux
  • avnet
  • petalinux2020
Related

Minized Petalinux 2020 - WiFi Shell Script

apadana1984
apadana1984 over 6 years ago

Hello,

 

I am building Petalinux 2020.1 for my Minized Board. I downloaded the Avnet BSP package. I noticed that the default Shell script for enabling the WiFi module has an issue:

 

#Mount the eMMC

echo "Mount the eMMC."

mount /dev/mmcblk1p1 /mnt

 

When I boot my Petalinux, there is not such "mmcblk1p1". There is "mmcblk0p1". What is the best way to correct this file? I changed it and re-built my Petalinux, however, the shell script in the image file didn't change!!! Am I missing something?

 

Also, I changed my "wpa_supplicant.conf" file to include my WiFi user ID&PASSWD, however, the file doesn't change in the linux image file.

 

I appreciate if someone can look into this problem.

 

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • narrucmot
    narrucmot over 6 years ago +1 suggested
    Hi Iman, That shell script (wifi.sh?) has been used for years, so I am surprised that it is breaking now. I will look into this. The reason why the script reverts to its original state on a reboot is because…
Parents
  • apadana1984
    0 apadana1984 over 6 years ago

    I fixed the issues as follows:

     

    1- Regarding the wifi.sh script, I changed the script to:

     

    #Overwrite the default wpa_supplicant setup with one edited with

    #the WLAN SSID and password that was previously copied to the eMMC.

    echo "Copy the wpa_supplicant.conf file from eMMC to /etc."

    echo "NOTE!  This file must have been previously edited with"

    echo "the WLAN SSID and password!"

    #Mount the eMMC

    echo "Copy the wpa_supplicant.conf file from eMMC to /etc."

    cp -f /media/sd-mmcblk0p2/usr/local/bin/wpa_supplicant.conf /etc/.

     

    #Run wpa_supplicant for secure networking:

    echo "Bringup the WiFi interface."

     

    The files already exists in /media/sd-mmcblk0p2/usr/local/bin folder. We don't need to mount it again in order to use it. I removed those the lines related to mounting and un-mounting.

     

    2- As for non-updating the rootfs.wic even after I rebuild the Petalinux, I noticed that those in /pre-built/linux/images are not being updated, however, the one in /images/linux directory is in fact being updated.

     

    My Minized now loads the correct shell scripts and WiFi modules works perfect.

     

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • apadana1984
    0 apadana1984 over 6 years ago

    I fixed the issues as follows:

     

    1- Regarding the wifi.sh script, I changed the script to:

     

    #Overwrite the default wpa_supplicant setup with one edited with

    #the WLAN SSID and password that was previously copied to the eMMC.

    echo "Copy the wpa_supplicant.conf file from eMMC to /etc."

    echo "NOTE!  This file must have been previously edited with"

    echo "the WLAN SSID and password!"

    #Mount the eMMC

    echo "Copy the wpa_supplicant.conf file from eMMC to /etc."

    cp -f /media/sd-mmcblk0p2/usr/local/bin/wpa_supplicant.conf /etc/.

     

    #Run wpa_supplicant for secure networking:

    echo "Bringup the WiFi interface."

     

    The files already exists in /media/sd-mmcblk0p2/usr/local/bin folder. We don't need to mount it again in order to use it. I removed those the lines related to mounting and un-mounting.

     

    2- As for non-updating the rootfs.wic even after I rebuild the Petalinux, I noticed that those in /pre-built/linux/images are not being updated, however, the one in /images/linux directory is in fact being updated.

     

    My Minized now loads the correct shell scripts and WiFi modules works perfect.

     

    Thank you