Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design GPIO can be used as input/output port?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 355 subscribers
  • Views 1573 views
  • Users 0 members are here
Related

GPIO can be used as input/output port?

koseiyokoyama
koseiyokoyama over 2 years ago

I am trying to comunicate with Temp/Humid module DHT11
However data pin should be pull up to 3.3 but while my RTL trying to comunicate with DHT11 throgh IO13 pin, Data line pull down to GND.
if GPIO can be inout port, then any one know how?

My RTL working fine in simulation with Vivado

  • Sign in to reply
  • Cancel

Top Replies

  • embeddedguy
    embeddedguy over 2 years ago +2 suggested
    As you are using DHT11 sensor, you should use Serial protocol i.e. UART RX line to sample the received values. The DHT11 sensor works like following. "Data line remains in high normally, then master…
  • embeddedguy
    0 embeddedguy over 2 years ago

    As you are using DHT11 sensor, you should use Serial protocol i.e. UART RX line to sample the received values.

    The DHT11 sensor works like following.

    "Data line remains in high normally, then master in this case FPGA will start communication first. The the sensor will respond with temparature, humidity data".

    See the following image of timing diagram.

    image

    The output given out by the data pin will be in the order of 8bit humidity integer data + 8bit the Humidity decimal data +8 bit temperature integer data + 8bit fractional temperature data +8 bit parity bit. To request the DHT11 module to send these data the I/O pin has to be momentarily made low and then held high as shown in the timing diagram below

    components101.com/.../dht11-temperature-sensor

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago

    It seems a waste to use such a sensor directly attached to a MiniZed. There are better sensors, that interface through more normal interfaces.

    One typical approach to connect such a sensor, is to use two ports; one as input, and the other as output, and build yourself an interface. You'd have to check if the values below are appropriate (I've not read the DHT11 datasheet). With such an interface circuit, the controller (FPGA or microcontroller or otherwise, it's up to you) doesn't need to switch between input and output. 

    When a logic high is sent by the controller, the sensor line is pulled low. When a logic low is sent by the controller, the line is pulled up, and the remote sensor is free to pull the line low.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 2 years ago

    I think this has cropped up here before and is actually an issue with how the Vivado top-level wrapper works and how you get the tristate control (that I presume you're using to implement the open-drain) to propagate up from your code level, one step down from the wrapper. I seem to remember (vaguely) something about a specific naming convention you have to use for the two drive signals (output signal and tristate control) in order for Vivado to understand what you're asking for and create a wrapper with the tristate implemented up at the actual pin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 2 years ago in reply to jc2048

    The advantage of the external MOSFET approach is that the output of your FPGA is protected if you get things wrong. Most FPGAs don't offer a real open drain output so you end up having to never slip up with your code to avoid the FPGA sometimes pulling up an external active pull down.

    In the OP's case I'd recommend this since adding a MOSFET to his sensor is not a big deal.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 2 years ago in reply to jc2048

    Here's the thread that I dimly remembered, in case it's of any use to anyone:

    /technologies/fpga-group/f/forum/50650/vivado-and-zynq-tri-state-help/197015

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • koseiyokoyama
    0 koseiyokoyama over 2 years ago

    Thank you so many help!!

    I finally make my RTL working!

    the keys are

            use Global option when Generate output Objects...

            use PULLUP(inout signal port); 

                   assign inout_port = output_enable ? output_reg : 1'bZ;

                     in RTL

            use set_property PULLUP true [get_port inout_port] in xdc

    thanks again!!