Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design programming IDT clock
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 356 subscribers
  • Views 952 views
  • Users 0 members are here
  • picozed
Related

programming IDT clock

wm2015email
wm2015email over 5 years ago

Regarding,  "PicoZed SOM 7030 WITH FMC Carrier Card Version 2" board....

 

Daniel Rozwood was saying the IDT clock is programmable in a post entitled

"Re: power on reset frequency of pl_clk for PicoZed 7030 SOM + FMC Carrier V2"...

and that "Straight from the factory, the IDT clock is not programmed. You need to configure it and program it"

 

Let's say I want to create a design specifically for the purpose of programming the Clockchip on the board by

instantiating an I2C core in verilog and connect it to pins:

# I2C Peripherials on FMCV2 Board

  H6     fmc2_board_scl                 jx1_io_vr_n         .              35           LVCMOS18   inout

  H5     fmc2_board_sda                 jx1_io_vr_p         .              35           LVCMOS18   inout

 

But how can I use the I2C core without a  reference clock to drive the I2C core?

 

Specially, the I2C core needs to know the clock frequency that its connected to in order

to count the number of clock for each bit of the I2C to acheive 100 Khz clock rate....

 

Anyways, i didn't want to mess around with the reference design because its for a version of Vivado that I don't have and it takes hours to download on my network... and needing sufficent space on my harddrive etc... i figured how hard could it be to program a clock chip using an I2C bus...  but the delima is that therere's no fixed reference clock of any kind on the board... unless I put in the ZYNQ... which i also don't want to do because you need to invoke SDK to get the FCLK to start...

 

Is there some other reference clock pin on the FPGA that i don't know about, maybe i can get a clock from:

E9    ps_sd_clk                 jx3_ps_mio40 ?

 

Except i think this clock is also generated by Zynq...

  • Sign in to reply
  • Cancel
  • bhfletcher
    bhfletcher over 5 years ago

    It sounds like you are asking if there is a way to bring an external clock into the Zynq-7000 PL using PicoZed and the PicoZed FMC-V2 Carrier. For the PL, none of the MIO will work since those are only tied to the PS. I looked over the schematics, and I think the only option you have is to use one of the PL Pmods, but then you'd have to look if any of the PL Pmod I/Os are connected to clock-capable pins on the Zynq.

     

    Why not just take the boot.bin from the reference design and run it? That will program the EEPROM for you. You don't have to build anything or even open the tools. Just copy the boot.bin to the microSD card and boot SD. Here is the 7030 default boot.bin.

    sd_card_PZ7030_FMC2_DEFAULT_BOOT.zip

     

    Bryan