• Products and Partners
    Products and Partners
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
Avnet Boards Forums
  • Products and Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design GTX transceivers
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 357 subscribers
  • Views 3239 views
  • Users 0 members are here
Related

GTX transceivers

e14 Contributor
e14 Contributor over 11 years ago

Hi..

I am working with GTX transceivers on the 7030.  I am trying to configure the GTXE2_CHANNEL_X0Y1 transceiver attached to SMA on the Carrier board using Aurora 8b10b example design.
I instantiated the aurora_example design to the processing wrapper.  This only have the zynq processing with 2 pl_clocks required in Aurora.

In the file.xdc I am doing this configuration.  I donu00B4t know if it is right,
#######################################################
set_property PACKAGE_PIN U9 [get_ports GTXQ0_P]
set_false_path -through [get_pins -hier *cdc_to*]
set_property LOC GTXE2_CHANNEL_X0Y1 [get_cells aurora_module_i/aurora_8b10b_0_i/U0/gt_wrapper_i/aurora_8b10b_0_multi_gt_i/gt0_aurora_8b10b_0_i/gtxe2_i]
set_property DONT_TOUCH true [get_cells ProcessingSystem_i]
set_property DONT_TOUCH true [get_cells ProcessingSystem_i/processing_system7_0]
set_property DONT_TOUCH true [get_cells ProcessingSystem_i/processing_system7_0/inst]
set_property DONT_TOUCH true [get_cells ProcessingSystem_i/util_ds_buf_0]
set_property PACKAGE_PIN Y8 [get_ports RXN]
set_property PACKAGE_PIN W8 [get_ports RXP]
set_property PACKAGE_PIN Y4 [get_ports TXN]
set_property PACKAGE_PIN W4 [get_ports TXP]

#######################################################

I got this  error in the implementation, and I have no idea what is the reason:

[Place 30-378] Input pin of input buffer Communication_block/aurora_module_i/U0/clock_module_i/init_clk_ibufg_i has an illegal connection to a logic constant value.
[Place 30-99] Placer failed with error: 'Implementation Feasibility check failed, Please see the previously displayed individual error or warning messages for more details.'
Please review all ERROR, CRITICAL WARNING, and WARNING messages during placement to understand the cause for failure.

Please help


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Dan

    also my question is if, Do I have to use set_property XDC command to constrain the location of the GT reference clock pins ?
    Thanks a lot

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Dan

    also my question is if, Do I have to use set_property XDC command to constrain the location of the GT reference clock pins ?
    Thanks a lot