Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design GTX transceivers
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 357 subscribers
  • Views 3231 views
  • Users 0 members are here
Related

GTX transceivers

e14 Contributor
e14 Contributor over 11 years ago

Hi..

I am working with GTX transceivers on the 7030.  I am trying to configure the GTXE2_CHANNEL_X0Y1 transceiver attached to SMA on the Carrier board using Aurora 8b10b example design.
I instantiated the aurora_example design to the processing wrapper.  This only have the zynq processing with 2 pl_clocks required in Aurora.

In the file.xdc I am doing this configuration.  I donu00B4t know if it is right,
#######################################################
set_property PACKAGE_PIN U9 [get_ports GTXQ0_P]
set_false_path -through [get_pins -hier *cdc_to*]
set_property LOC GTXE2_CHANNEL_X0Y1 [get_cells aurora_module_i/aurora_8b10b_0_i/U0/gt_wrapper_i/aurora_8b10b_0_multi_gt_i/gt0_aurora_8b10b_0_i/gtxe2_i]
set_property DONT_TOUCH true [get_cells ProcessingSystem_i]
set_property DONT_TOUCH true [get_cells ProcessingSystem_i/processing_system7_0]
set_property DONT_TOUCH true [get_cells ProcessingSystem_i/processing_system7_0/inst]
set_property DONT_TOUCH true [get_cells ProcessingSystem_i/util_ds_buf_0]
set_property PACKAGE_PIN Y8 [get_ports RXN]
set_property PACKAGE_PIN W8 [get_ports RXP]
set_property PACKAGE_PIN Y4 [get_ports TXN]
set_property PACKAGE_PIN W4 [get_ports TXP]

#######################################################

I got this  error in the implementation, and I have no idea what is the reason:

[Place 30-378] Input pin of input buffer Communication_block/aurora_module_i/U0/clock_module_i/init_clk_ibufg_i has an illegal connection to a logic constant value.
[Place 30-99] Placer failed with error: 'Implementation Feasibility check failed, Please see the previously displayed individual error or warning messages for more details.'
Please review all ERROR, CRITICAL WARNING, and WARNING messages during placement to understand the cause for failure.

Please help


  • Sign in to reply
  • Cancel
  • drozwood90
    0 drozwood90 over 11 years ago

    Hi there,

    From the error message, it seems that you have a constant driving the clock input.
    Check that you have a clock input and are NOT passing the clock through any sort of constant or buffer that might logically turn the clock into a constant.

    Which Aurora example design are you using as your guide?

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hello Dan

    I am using Aurora 8b10b example_design.  I am using the PS only for getting the clocks required for Aurora:  INIT_ClK_N, INIT_CLOCK_P and DRP_CLK_IN.  For the differential init_clock I used a Utility Differential IO Buffer (OBUF_DS_P and OBUF_DS_N outputs).

    Thanks for the help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Do I have to put in the <file>.xdc the constrain  for the gtx module connected for SMA port ????. In this case I am using the X0Y1

    set_property LOC GTXE2_CHANNEL_X0Y1 [get_cells aurora_module_i/aurora_8b10b_0_i/U0/gt_wrapper_i/aurora_8b10b_0_multi_gt_i/gt0_aurora_8b10b_0_i/gtxe2_i]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Dan

    also my question is if, Do I have to use set_property XDC command to constrain the location of the GT reference clock pins ?
    Thanks a lot

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Please help

    I am running IBERT module with ZC030, the results looks right, but I canu00B4t see BER result, it does not show any data.
    , I am using the transceiver connected to SMA.. and the Errors are show as 0E0.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 11 years ago

    Hi there,

    -what is your clock source?  If you are using the PS for clocks for the Aurora design, what is driving the MGTClock pin?
    -You do not HAVE to put the constraint in there, but it is highly recommended in order to force the place and route to properly prioritize fabric resources during place and route
    -The MGT pins are hard pins, just as the MGT TX/RX pins are.  I do not think you need to define them in the XDC
    -What is the configuration you are using for the IBERT design?  Clock Input Freq., Clock input Pin (0 or 1), expected data rate?
    If errors is 0e0, then you are not getting errors.  That is a good thing.  What is more important is the BER.  WHat does that show?  I know you said you can't see BER result, but what do you mean?  The cell in the column is empty?  It is too big?  Too Small?
    -does the IBERT design say it has established link?
    -Have you connected the TX_P to RX_P and TX_N to RX_N?
    -are your cables rated for the speed that you are running?

    You can view this series of tech tips, which will help SHOW you what I mean and also help walk you through double checking all the little things.
    Go to: http://picozed.org/support/trainings-and-videos
    Search for:
    Tech Tip - Transceiver Tools 101: Intro to IBERT
    Tech Tip - Transceiver Tools 102: We have an IBERT bit stream, now what?
    Tech Tip - Transceiver Tools 103: Now that we are running, what are all these adjustments?
    Tech Tip - Transceiver Tools 104: Getting More Margin

    I think the one that is going to help you the most is 102 - which will help double check all the connections and setup.  Then you can proceed through the rest of the videos.  The last video walks you through how to get an EYE-Diagram, which will give us a good indication about what is going on.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 11 years ago

    Also,

    IBERT will take care of all the constraints for youl

    The only thing is will not account for is the SFP Laser Enable pin.  I am working on an automated design that will do this for you.  You are using a PicoZed 7030?  I just want to ensure I am pointing you to the proper source material!

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Dan
    Aurora
    I am using PS clock for the differential clock (INIT_ClK_N, INIT_CLOCK_P) and DRP_CLK_IN both 50Mhz.  These are required for Aurora module.
    For the  MGTClock  I am connecting  to MGTREFCLK0_P and MGTREFCLK0_N (U9, V9).
    ---------------------------------------------
    IBERT
    Yes, I am using PicoZed 7030, with the FMC Card.
    I have followed all the steps in the videos and simulated using Vivado 2015.1 and 2014.4, but the results are the same.
    - I am using 3.125 Gbps and Refclk 250MHz.. For the FMC card SW9 and SW10  in OFF OFF OFF ON ON OFF positions for setting 250 MHz.
    - In Refclk Selection I put MGTREFCLK1 112 with QUAD112 1 and DIFF SSTL12 Standard.
    - The link is established also it shows Locked.. When I program the board, it founds the physical SMA link connection.

    -The BER column is empty.
    - I did the same test for Kintex 7, and I am having the same problem  (BER column is empty), and also Errors column is 0E0 for the SMA.
    - Of course I connected the cables (TXN - RXN) and (TXP - RXP)
    I havenu00B4t rated my cables for this speed. Could be the reason for not getting BER result even when Errors are 0E0 ??

    Thanks a lot

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 11 years ago in reply to e14 Contributor

    Unless you mistyped, I think I found your issue.
    If you are using a clock on MDTREFCLK0, you need to select that clock input when walking through the configuration.  For the videos, I chose to use the onboard clock.
    If your cables are not rated for this speed, you will likely see too many errors and struggle getting link.  From your description, I do not think that the speed rating of the cables is the issue.  However, I have seen similar issues when using a BAD cable.  At these rates, it does not take much to make a cable not function well.

    When you tested with the Kintex 7, did you use the same cables?

    What are you using for the JTAG connector?

    It seems that you have the configuration setup properly for the onboard clock.
    *Ensure that the Protocol Selection tab, you choose MGTREFCLK1 112 with a Custom 1 / 3.125 Gbps protocol.
    *In the Clock settings tab, choose Quad112 1 from the pull down under Source.  The I/O standard should grey out.  If it does not, single click it.  This might not do anything, but that is what I typically do.

    Since you are not seeing any connection errors over JTAG, there must be SOME kind of clock.  This list is more to double check your setup:
    *Please check that there is NO jumper on JP6 (to the left of the SW9 and SW10), this selects the clock input source mux (see sheet 3 of the schematic)
    *Since you have a 7030 based PicoZed, ensure there are NO jumpers installed on CON2.  If you select anything except 1.8V this will damage the PicoZed 7030.
    *try different coax cables - it is possible that you have a bad cable (I have experienced this)
    *Make sure the coax cables are SNUG, if not you could have issues from that
    **having Link show only says that there are enough bits flowing, the device knows something is probably there, if you do not have grounding caps on the various connectors, the capacitive effect of the board can cause this

    In video 104, I describe more of the tweaking features.  You can try clicking the inject error button for the SMA channel.  This will force errors into the stream.  If this does not work, then we need to ensure the transceivers are working.

    At this point, let's enable the loopback (see video 103 around 2:25 seconds).  Try the Near End PCS and then Near End PMA.
    *If you enable Near End PCS and you do not see the everything start to work, I would delete the design and start over.  Near End PCS loops back the transceiver data digitally.  If this does not work, nothing will.
    *Using Near End PMA will allow you to test the Zynq transceivers up through the analog part of the chip, without leaving the chip.  This will ensure that the chip is good.

    If these both check out as AOK, I would then unseat and reseat the PicoZed on your carrier card as well as change your cables (if you have not already).

    Please let me know how this helps.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to drozwood90

    Hi Dan

    -Yes, I used the same cable for testing Kintex 7.
    -For JTAG connector in the FMC Carrier I am using HS2 Rev. A
    -I am using the configuration that you are describing.
    -I donu00B4t use jumper in JP6 neither CON2.
    -I tried different cables,  and the problem is the same. I made sure the coax cable were snug. 
    - When I inject error using the button, I can see error count increased in the Error Column.
    -Near End PCS and then Near End PMA works, using all 4 transceivers.
    -Also I build a new project in Vivado 2014.4 with Ubuntu, and the result is the same.
    However I found out that in the RX Properties Window, RX_BER had values and are changed. but BER, TXUSERCLK, TXUSERCLK2, RXUSERCLK, TXUSERCLK2 columns are always empty.
    These are the data display it:
    NametValue
    CLASSthw_sio_rx
    DISPLAY_NAMEtMGT_X0Y1/RX
    DRP.ES_CONTROLt00
    DRP.ES_CONTROL_STATUSt1
    DRP.ES_ERRDET_ENt0
    DRP.ES_ERROR_COUNTt0000
    DRP.ES_EYE_SCAN_ENt1
    DRP.ES_HORZ_OFFSETt000
    DRP.ES_PMA_CFGt000
    DRP.ES_PRESCALEt00
    DRP.ES_QUALIFIERt00000000000000000000
    DRP.ES_QUAL_MASKt00000000000000000000
    DRP.ES_RDATAt00000000000000000000
    DRP.ES_SAMPLE_COUNTt0000
    DRP.ES_SDATAt00000000000000000000
    DRP.ES_SDATA_MASKt00000000000000000000
    DRP.ES_UT_SIGNt0
    DRP.ES_VERT_OFFSETt000
    DRP.FTS_DESKEW_SEQ_ENABLEtF
    DRP.FTS_LANE_DESKEW_CFGtF
    DRP.FTS_LANE_DESKEW_ENt0
    DRP.RXBUFRESET_TIMEt01
    DRP.RXBUF_ADDR_MODEt1
    DRP.RXBUF_EIDLE_HI_CNTt8
    DRP.RXBUF_EIDLE_LO_CNTt0
    DRP.RXBUF_ENt1
    DRP.RXBUF_RESET_ON_CB_CHANGEt1
    DRP.RXBUF_RESET_ON_COMMAALIGNt0
    DRP.RXBUF_RESET_ON_EIDLEt0
    DRP.RXBUF_RESET_ON_RATE_CHANGEt1
    DRP.RXBUF_THRESH_OVFLWt3D
    DRP.RXBUF_THRESH_OVRDt0
    DRP.RXBUF_THRESH_UNDFLWt04
    DRP.RXCDRFREQRESET_TIMEt01
    DRP.RXCDRPHRESET_TIMEt01
    DRP.RXCDR_CFGt03800023FF40200020
    DRP.RXCDR_FR_RESET_ON_EIDLEt0
    DRP.RXCDR_HOLD_DURING_EIDLEt0
    DRP.RXCDR_LOCK_CFGt15
    DRP.RXCDR_PH_RESET_ON_EIDLEt0
    DRP.RXDFELPMRESET_TIMEt0F
    DRP.RXDLY_CFGt001F
    DRP.RXDLY_LCFGt030
    DRP.RXDLY_TAP_CFGt0000
    DRP.RXGEARBOX_ENt0
    DRP.RXISCANRESET_TIMEt01
    DRP.RXLPM_HF_CFGt00F0
    DRP.RXLPM_LF_CFGt00F0
    DRP.RXOOB_CFGt06
    DRP.RXOUT_DIVt1
    DRP.RXPCSRESET_TIMEt01
    DRP.RXPHDLY_CFGt084020
    DRP.RXPH_CFGt000000
    DRP.RXPH_MONITOR_SELt00
    DRP.RXPMARESET_TIMEt03
    DRP.RXPRBS_ERR_LOOPBACKt0
    DRP.RXSLIDE_AUTO_WAITt7
    DRP.RXSLIDE_MODEt0
    DRP.RX_BIAS_CFGt004
    DRP.RX_BUFFER_CFGt00
    DRP.RX_CLK25_DIVt09
    DRP.RX_CLKMUX_PDt1
    DRP.RX_CM_SELt3
    DRP.RX_CM_TRIMt4
    DRP.RX_DATA_WIDTHt4
    DRP.RX_DDI_SELt00
    DRP.RX_DEBUG_CFGt000
    DRP.RX_DEFER_RESET_BUF_ENt1
    DRP.RX_DFE_CTLE_STAGE1t8
    DRP.RX_DFE_CTLE_STAGE2t3
    DRP.RX_DFE_CTLE_STAGE3t0
    DRP.RX_DFE_GAIN_CFGt020FEA
    DRP.RX_DFE_H2_CFGt000
    DRP.RX_DFE_H3_CFGt040
    DRP.RX_DFE_H4_CFGt0F0
    DRP.RX_DFE_H5_CFGt0E0
    DRP.RX_DFE_KL_CFG2t3010D90C
    DRP.RX_DFE_KL_CFGt00FE
    DRP.RX_DFE_LPM_CFGt0954
    DRP.RX_DFE_LPM_HOLD_DURING_EIDLEt0
    DRP.RX_DFE_UT_CFGt11E00
    DRP.RX_DFE_VP_CFGt03F03
    DRP.RX_DFE_XYD_CFGt0000
    DRP.RX_DISPERR_SEQ_MATCHt1
    DRP.RX_INT_DATAWIDTHt1
    DRP.RX_OS_CFGt0080
    DRP.RX_SIG_VALID_DLYt09
    DRP.RX_XCLK_SELt0
    DRP.TXBUF_RESET_ON_RATE_CHANGEt0
    DRP.TXPCSRESET_TIMEt01
    DRP.TXPMARESET_TIMEt01
    DRP.TX_LOOPBACK_DRIVE_HIZt0
    DRP.TX_RXDETECT_CFGt1832
    DRP.TX_RXDETECT_REFt4
    ES_HORZ_MIN_MAXt64
    LINE_RATEt3.125
    LOGIC.ERRBIT_COUNTt000000000000
    LOGIC.GT_SOURCES_SYSCLKt0
    LOGIC.LINKt1
    LOGIC.MGT_ERRCNT_RESET_CTRLt0
    LOGIC.MGT_ERRCNT_RESET_STATt0
    LOGIC.MGT_RESET_CTRLt0
    LOGIC.MGT_RESET_STATt0
    LOGIC.RXPAT_IDt1
    LOGIC.RXRECCLK_FREQ_CNTt0F9F
    LOGIC.RXRECCLK_FREQ_TUNEt4000
    LOGIC.RXUSRCLK2_FREQ_CNTt0FA0
    LOGIC.RXUSRCLK2_FREQ_TUNEt4000
    LOGIC.RXUSRCLK_FREQ_CNTt0FA0
    LOGIC.RXUSRCLK_FREQ_TUNEt4000
    LOGIC.RXWORD_COUNTt000844861ACB
    LOGIC.RX_DCM_LOCKt1
    LOGIC.RX_DCM_RESET_CTRLt0
    LOGIC.RX_DCM_RESET_STATt0
    LOGIC.RX_FRAMEDt0
    LOGIC.TX_DCM_RESET_CTRLt0
    LOGIC.TX_DCM_RESET_STATt1
    LOOPBACKtNone
    NAMEtlocalhost/xilinx_tcf/Digilent/210249982432/1_1/IBERT/Quad_112/MGT_X0Y1/RX
    PARENTtlocalhost/xilinx_tcf/Digilent/210249982432/1_1/IBERT/Quad_112/MGT_X0Y1
    PORT.CFGRESETt0
    PORT.CPLLRESETt0
    PORT.EYESCANDATAERRORt0
    PORT.EYESCANMODEt0
    PORT.EYESCANRESETt0
    PORT.EYESCANTRIGGERt0
    PORT.GTRESETSELt0
    PORT.GTRXRESETt0
    PORT.GTTXRESETt0
    PORT.LOOPBACKt0
    PORT.RESETOVRDt0
    PORT.RX8B10BENt0
    PORT.RXBUFRESETt0
    PORT.RXBUFSTATUSt0
    PORT.RXBYTEISALIGNEDt0
    PORT.RXBYTEREALIGNt0
    PORT.RXCDRFREQRESETt0
    PORT.RXCDRHOLDt0
    PORT.RXCDRLOCKt1
    PORT.RXCDROVRDENt0
    PORT.RXCDRRESETt0
    PORT.RXCDRRESETRSVt0
    PORT.RXCHANBONDSEQt0
    PORT.RXCHANISALIGNEDt1
    PORT.RXCHANREALIGNt0
    PORT.RXCHARISCOMMAt00
    PORT.RXCHARISKt00
    PORT.RXCHBONDENt0
    PORT.RXCHBONDIt10
    PORT.RXCHBONDLEVELt0
    PORT.RXCHBONDMASTERt0
    PORT.RXCHBONDOt00
    PORT.RXCHBONDSLAVEt0
    PORT.RXCLKCORCNTt0
    PORT.RXCOMINITDETt0
    PORT.RXCOMMADETt0
    PORT.RXCOMMADETENt0
    PORT.RXCOMSASDETt0
    PORT.RXCOMWAKEDETt0
    PORT.RXDATAVALIDt1
    PORT.RXDDIENt0
    PORT.RXDFEAGCHOLDt0
    PORT.RXDFEAGCOVRDENt0
    PORT.RXDFECM1ENt0
    PORT.RXDFELFHOLDt0
    PORT.RXDFELFOVRDENt0
    PORT.RXDFELPMRESETt0
    PORT.RXDFETAP2HOLDt0
    PORT.RXDFETAP2OVRDENt0
    PORT.RXDFETAP3HOLDt0
    PORT.RXDFETAP3OVRDENt0
    PORT.RXDFETAP4HOLDt0
    PORT.RXDFETAP4OVRDENt0
    PORT.RXDFETAP5HOLDt0
    PORT.RXDFETAP5OVRDENt0
    PORT.RXDFEUTHOLDt0
    PORT.RXDFEUTOVRDENt0
    PORT.RXDFEVPHOLDt0
    PORT.RXDFEVPOVRDENt0
    PORT.RXDFEVSENt0
    PORT.RXDFEXYDENt0
    PORT.RXDFEXYDHOLDt0
    PORT.RXDFEXYDOVRDENt0
    PORT.RXDISPERRt00
    PORT.RXDLYBYPASSt1
    PORT.RXDLYENt0
    PORT.RXDLYOVRDENt0
    PORT.RXDLYSRESETt0
    PORT.RXDLYSRESETDONEt0
    PORT.RXELECIDLEt1
    PORT.RXELECIDLEMODEt0
    PORT.RXGEARBOXSLIPt0
    PORT.RXHEADERt0
    PORT.RXHEADERVALIDt0
    PORT.RXLPMENt0
    PORT.RXLPMHFHOLDt0
    PORT.RXLPMHFOVRDENt0
    PORT.RXLPMLFHOLDt0
    PORT.RXLPMLFKLOVRDENt0
    PORT.RXMCOMMAALIGNENt0
    PORT.RXMONITOROUTt7F
    PORT.RXMONITORSELt0
    PORT.RXNOTINTABLEtFF
    PORT.RXOOBRESETt0
    PORT.RXOSHOLDt0
    PORT.RXOSOVRDENt0
    PORT.RXOUTCLKFABRICt1
    PORT.RXOUTCLKPCSt0
    PORT.RXOUTCLKSELt1
    PORT.RXPCOMMAALIGNENt0
    PORT.RXPCSRESETt0
    PORT.RXPDt0
    PORT.RXPHALIGNt0
    PORT.RXPHALIGNDONEt0
    PORT.RXPHALIGNENt0
    PORT.RXPHDLYPDt0
    PORT.RXPHDLYRESETt0
    PORT.RXPHMONITORt00
    PORT.RXPHOVRDENt0
    PORT.RXPHSLIPMONITORt09
    PORT.RXPMARESETt0
    PORT.RXPOLARITYt0
    PORT.RXPRBSCNTRESETt0
    PORT.RXPRBSERRt0
    PORT.RXPRBSSELt0
    PORT.RXQPIENt0
    PORT.RXQPISENNt0
    PORT.RXQPISENPt0
    PORT.RXRATEt0
    PORT.RXRATEDONEt0
    PORT.RXRESETDONEt1
    PORT.RXSLIDEt0
    PORT.RXSTARTOFSEQt0
    PORT.RXSTATUSt4
    PORT.RXSYSCLKSELt3
    PORT.RXUSERRDYt1
    PORT.RXVALIDt0
    PORT.TXDETECTRXt0
    PORT.TXDLYSRESETt0
    PORT.TXDLYSRESETDONEt0
    PORT.TXPCSRESETt0
    PORT.TXPHDLYRESETt0
    PORT.TXPMARESETt0
    PORT.TXRESETDONEt1
    RXDFEENABLEDt1
    RXOUTCLKSELtRXOUTCLKPCS
    RXOUT_DIVt2
    RXPLLtQPLL
    RXRATEtUse RX_OUT_DIV
    RXTERMt900 mV
    RXTERMMODEtProgrammable
    RXUSRCLK2_FREQt97,680664
    RXUSRCLK_FREQt97,680664
    RX_BERt8,8004921487762598e-13
    RX_DATA_WIDTHt32
    RX_DFE_CTLEt
    RX_INTERNAL_DATAPATHt4-byte
    RX_PATTERNtPRBS 7-bit
    RX_PLLtlocalhost/xilinx_tcf/Digilent/210249982432/1_1/IBERT/Quad_112/COMMON_X0Y0/QPLL_0
    RX_RECEIVED_BIT_COUNTt1136300087648
    STATUSt3.125 Gbps

    When I tried Create Scan, also doesnu00B4t wok.
    At this point, no idea what else I could do ...

    Do you have another suggestion please?. I appreciate a lot your kindly help.






    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>