Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design 1.2V common mode LVDS
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 356 subscribers
  • Views 440 views
  • Users 0 members are here
Related

1.2V common mode LVDS

e14 Contributor
e14 Contributor over 11 years ago

I am evaluating the PicoZed to interface to a sensor with a 1.2V common mode LVDS SPI bus interface (so 8 pins) and then a handful of CMOS 3.3V IO pins for control.

Assuming that a 1.8V rail voltage will work for the LVDS, I am asking if I can do this without the carrier board and using the 7010 PicoZed with PS-based IO.

Bank 500 has 8 PS IO lines on JX2 at 3.3V. This looks good for the few CMOS lines.
Bank 501 has 12 PS IO lines on JX3 at 1.8V. But can I implement differential signaling easily on the PS side, or do I need to do this with one of the PL banks?

Any thoughts?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago

    The MIOs are not differential capable. You will need to use the PL. You could still use a SPI controller from the PS, interfaced through EMIO into the PL, with a shim to go from single-ended to differential on the PL IOs.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 10 years ago

    The MIOs are not differential capable. You will need to use the PL. You could still use a SPI controller from the PS, interfaced through EMIO into the PL, with a shim to go from single-ended to differential on the PL IOs.

    Bryan