Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design board selection question
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 800 views
  • Users 0 members are here
Related

board selection question

e14 Contributor
e14 Contributor over 11 years ago

I like to purchase a development board for personal use, mainly to learn on the embedded processor side under petalinux.  any recommendations? nothing too expensive.  what the main difference between pico/micro board other than size?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi s002wjh,

    For anyone looking to get started with Zynq, MicroZed is hands-down one of the best low-cost options out there.  By purchasing the Eval Kit (look for part number  AES-Z7MB-7Z010-G) you get a board that you can do embedded processor work on without needing a carrier board for 199USD.

    http://microzed.org/buy

    If you decide to move onto doing work with the programmable logic, you can still do this without a carrier.  The point at which you need a carrier is when you want to start using the programmable logic AND the flexible IOs that are attached to it.

    At that point, if you are simply doing simple circuit prototyping, you might be able to utilize a MicroZed Breakout Carrier for 59 USD.

    If you are looking to do low-cost peripherals like Pmods, then it is recommended that you look at the MicroZed I/O Carrier for 149 USD.

    If you are looking to do high performance FMC expansion modules, then you will want to look at the MicroZed FMC Carrier for 149 USD.

    The board sizes between MicroZed and PicoZed are actually the same.  For PicoZed, many of the outside world connectors have been moved down to the carrier board so the PicoZed SOM has a lower vertical profile than MicroZed.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    hi is AES-Z7MB-7Z010-G  this microzed SBC?

    http://microzed.org/product/microzed-sbc

    the buy option only has part#, doesn't has description

    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    This part number is the MicroZed Evaluation kit, which includes a 'standard' commercial temp 7010 MicroZed along with a node/device locked Xilinx Vivado tool voucher, a microSD Card and a MicroUSB cable. http://microzed.org/sites/default/files/PB-AES-Z7MB-7Z010-G-v3.pdf

     

    AES-Z7MB-7Z010-SBC-G is the part number for a commercial temp 7010 MicroZed SBC SOM. It is the SOM only with no SD Card, cable or voucher.  It is listed in a separate section on the 'Buy' page just below the MicroZed section.

     

    If you click the 'Buy' button it will take you to a page with a description.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    This part number is the MicroZed Evaluation kit, which includes a 'standard' commercial temp 7010 MicroZed along with a node/device locked Xilinx Vivado tool voucher, a microSD Card and a MicroUSB cable. http://microzed.org/sites/default/files/PB-AES-Z7MB-7Z010-G-v3.pdf

     

    AES-Z7MB-7Z010-SBC-G is the part number for a commercial temp 7010 MicroZed SBC SOM. It is the SOM only with no SD Card, cable or voucher.  It is listed in a separate section on the 'Buy' page just below the MicroZed section.

     

    If you click the 'Buy' button it will take you to a page with a description.

     

    -Gary