Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Failed to program picozed7015
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 582 views
  • Users 0 members are here
Related

Failed to program picozed7015

e14 Contributor
e14 Contributor over 9 years ago

I'm using custom carrier with pico-7015 board.

 

I have a working carrier and a bootable SD card.  When I load the SD card into new carrier board then power on, the DONE led in the carrier will blink at a frequency of several seconds. I have tried JTAG, but it returned "ERROR: [Labtools 27-3165] End of startup status: LOW".

The difference between new carrier board and the working carrier board is power related, IOs are the same. 

Now i don't know if it is a soldering problem or a configuration problem. What i am sure is that the power of 5V and 3.3V are both good, and there is no voltage drop.

Please give me some advices! Thanks ! 

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Wujingbang,

    When you state you have a working carrier Card, are you refering to an Avnet FMC Carrier Card or a different custom carrier card of yours? 

    Also take a look at this post https://forums.xilinx.com/t5/Welcome-Join/Error-Labtools-27-3165-End-of-startup-status-LOW/td-p/737029

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Thank you for replying. I have figured it out. The PG_MODULE pin in our carrier board is wrongly connected to the reset pin of a PCIE connector. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer