Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Picozed GTX  example design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 357 subscribers
  • Views 1615 views
  • Users 0 members are here
Related

Picozed GTX  example design

e14 Contributor
e14 Contributor over 10 years ago

Hi..

I am working with GTX transceivers on the Picozed 7030 using 10GBASE-R example design for 4-lane with VIVADO 2015.1. It refers the Kintex-7 FPGA Transceiver Wizard Example Design.

In the file.xdc I am doing this configuration. I don't know if it is right,
####################################################################
create_clock -period 6.400 [get_ports Q0_CLK1_GTREFCLK_PAD_P_IN]

create_clock -period 16.667 -name drpclk_in_i [get_ports DRP_CLK_IN_P]

# User Clock Constraints

set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_txfsmresetdone_r*/CLR}]
set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_txfsmresetdone_r*/D}]
set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_rxresetdone_vio_r*/CLR}]
set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_rxresetdone_vio_r*/D}]

set_property PACKAGE_PIN U5 [get_ports Q0_CLK1_GTREFCLK_PAD_P_IN]
set_property PACKAGE_PIN V5 [get_ports Q0_CLK1_GTREFCLK_PAD_N_IN]

set_property LOC GTXE2_CHANNEL_X0Y0 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt0_gtwizard_0_i/gtxe2_i]

set_property LOC GTXE2_CHANNEL_X0Y1 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt1_gtwizard_0_i/gtxe2_i]

set_property LOC GTXE2_CHANNEL_X0Y2 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt2_gtwizard_0_i/gtxe2_i]

set_property LOC GTXE2_CHANNEL_X0Y3 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt3_gtwizard_0_i/gtxe2_i]

##---------- Set ASYNC_REG for flop which have async input ----------
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt0_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt0_frame_check*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt1_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt1_frame_check*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt2_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt2_frame_check*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt3_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt3_frame_check*system_reset_r_reg}]

##---------- Set False Path from one clock to other ----------

set_property IOSTANDARD LVDS [get_ports DRP_CLK_IN_P]
set_property IOSTANDARD LVCMOS18 [get_ports TRACK_DATA_OUT]

set_property PACKAGE_PIN U2 [get_ports DRP_CLK_IN_P]
set_property PACKAGE_PIN R8 [get_ports TRACK_DATA_OUT]
set_property C_CLK_INPUT_FREQ_HZ 300000000 [get_debug_cores dbg_hub]
set_property C_ENABLE_CLK_DIVIDER false [get_debug_cores dbg_hub]
set_property C_USER_SCAN_CHAIN 1 [get_debug_cores dbg_hub]
connect_debug_port dbg_hub/clk [get_nets DRPCLK_IN]

#######################################################################
I got this error in the implementation, and I have no idea what is the reason:
ERROR: [Labtools 27-1395] Unable to arm ILA 'hw_ila_5'. The core clock is slow or no core clock connected for this ILA or the ILA core may not meet timing.
ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.

Please help.

--Huey

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    the other errors:

    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Labtools 27-3175] Target jsn-DLC9-Port_#0002.Hub_#0001 is no longer available.
    Please use disconnect_hw_server to close the current server connection. Check cable connectivity and that the target board is powered up.
    Restart the hw_server application running on host localhost, port 3121 and then use connect_hw_server to re-establish connection to target.

    Please help

    --Huey

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    the other errors:

    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.
    ERROR: [Labtools 27-3175] Target jsn-DLC9-Port_#0002.Hub_#0001 is no longer available.
    Please use disconnect_hw_server to close the current server connection. Check cable connectivity and that the target board is powered up.
    Restart the hw_server application running on host localhost, port 3121 and then use connect_hw_server to re-establish connection to target.

    Please help

    --Huey