Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Picozed GTX  example design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 357 subscribers
  • Views 1615 views
  • Users 0 members are here
Related

Picozed GTX  example design

e14 Contributor
e14 Contributor over 10 years ago

Hi..

I am working with GTX transceivers on the Picozed 7030 using 10GBASE-R example design for 4-lane with VIVADO 2015.1. It refers the Kintex-7 FPGA Transceiver Wizard Example Design.

In the file.xdc I am doing this configuration. I don't know if it is right,
####################################################################
create_clock -period 6.400 [get_ports Q0_CLK1_GTREFCLK_PAD_P_IN]

create_clock -period 16.667 -name drpclk_in_i [get_ports DRP_CLK_IN_P]

# User Clock Constraints

set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_txfsmresetdone_r*/CLR}]
set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_txfsmresetdone_r*/D}]
set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_rxresetdone_vio_r*/CLR}]
set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_rxresetdone_vio_r*/D}]

set_property PACKAGE_PIN U5 [get_ports Q0_CLK1_GTREFCLK_PAD_P_IN]
set_property PACKAGE_PIN V5 [get_ports Q0_CLK1_GTREFCLK_PAD_N_IN]

set_property LOC GTXE2_CHANNEL_X0Y0 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt0_gtwizard_0_i/gtxe2_i]

set_property LOC GTXE2_CHANNEL_X0Y1 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt1_gtwizard_0_i/gtxe2_i]

set_property LOC GTXE2_CHANNEL_X0Y2 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt2_gtwizard_0_i/gtxe2_i]

set_property LOC GTXE2_CHANNEL_X0Y3 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt3_gtwizard_0_i/gtxe2_i]

##---------- Set ASYNC_REG for flop which have async input ----------
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt0_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt0_frame_check*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt1_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt1_frame_check*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt2_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt2_frame_check*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt3_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt3_frame_check*system_reset_r_reg}]

##---------- Set False Path from one clock to other ----------

set_property IOSTANDARD LVDS [get_ports DRP_CLK_IN_P]
set_property IOSTANDARD LVCMOS18 [get_ports TRACK_DATA_OUT]

set_property PACKAGE_PIN U2 [get_ports DRP_CLK_IN_P]
set_property PACKAGE_PIN R8 [get_ports TRACK_DATA_OUT]
set_property C_CLK_INPUT_FREQ_HZ 300000000 [get_debug_cores dbg_hub]
set_property C_ENABLE_CLK_DIVIDER false [get_debug_cores dbg_hub]
set_property C_USER_SCAN_CHAIN 1 [get_debug_cores dbg_hub]
connect_debug_port dbg_hub/clk [get_nets DRPCLK_IN]

#######################################################################
I got this error in the implementation, and I have no idea what is the reason:
ERROR: [Labtools 27-1395] Unable to arm ILA 'hw_ila_5'. The core clock is slow or no core clock connected for this ILA or the ILA core may not meet timing.
ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.

Please help.

--Huey

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    Could you tell me what clock drives your logic?  Pasting your port definition is not really useful as we need to determine what clock drives the logic.

    You said you are using a 60MHz clock that feeds the PS.  What clocks have you brought out to the PL?  What is FCLK_CLK0 configured as? Since that appears to be the clock needed for your entities, what is it connected to?  You need to explicitly define those as well as the connection between.  It is rather easy to do in the Block Design wizard to create the clock. Then you would need to define that clock in the XDC for use with your code.  Lastly, actually connect the wire for that clock to the port input that you need it to be attached to.  Have you done that?

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    Could you tell me what clock drives your logic?  Pasting your port definition is not really useful as we need to determine what clock drives the logic.

    You said you are using a 60MHz clock that feeds the PS.  What clocks have you brought out to the PL?  What is FCLK_CLK0 configured as? Since that appears to be the clock needed for your entities, what is it connected to?  You need to explicitly define those as well as the connection between.  It is rather easy to do in the Block Design wizard to create the clock. Then you would need to define that clock in the XDC for use with your code.  Lastly, actually connect the wire for that clock to the port input that you need it to be attached to.  Have you done that?

    --Dan