Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Picozed GTX  example design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 357 subscribers
  • Views 1613 views
  • Users 0 members are here
Related

Picozed GTX  example design

e14 Contributor
e14 Contributor over 10 years ago

Hi..

I am working with GTX transceivers on the Picozed 7030 using 10GBASE-R example design for 4-lane with VIVADO 2015.1. It refers the Kintex-7 FPGA Transceiver Wizard Example Design.

In the file.xdc I am doing this configuration. I don't know if it is right,
####################################################################
create_clock -period 6.400 [get_ports Q0_CLK1_GTREFCLK_PAD_P_IN]

create_clock -period 16.667 -name drpclk_in_i [get_ports DRP_CLK_IN_P]

# User Clock Constraints

set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_txfsmresetdone_r*/CLR}]
set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_txfsmresetdone_r*/D}]
set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_rxresetdone_vio_r*/CLR}]
set_false_path -to [get_pins -hierarchical -filter {NAME =~ *_rxresetdone_vio_r*/D}]

set_property PACKAGE_PIN U5 [get_ports Q0_CLK1_GTREFCLK_PAD_P_IN]
set_property PACKAGE_PIN V5 [get_ports Q0_CLK1_GTREFCLK_PAD_N_IN]

set_property LOC GTXE2_CHANNEL_X0Y0 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt0_gtwizard_0_i/gtxe2_i]

set_property LOC GTXE2_CHANNEL_X0Y1 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt1_gtwizard_0_i/gtxe2_i]

set_property LOC GTXE2_CHANNEL_X0Y2 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt2_gtwizard_0_i/gtxe2_i]

set_property LOC GTXE2_CHANNEL_X0Y3 [get_cells gtwizard_0_support_i/gtwizard_0_init_i/inst/gtwizard_0_i/gt3_gtwizard_0_i/gtxe2_i]

##---------- Set ASYNC_REG for flop which have async input ----------
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt0_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt0_frame_check*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt1_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt1_frame_check*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt2_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt2_frame_check*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt3_frame_gen*system_reset_r_reg}]
##set_property ASYNC_REG TRUE [get_cells -hier -filter {name=~*gt3_frame_check*system_reset_r_reg}]

##---------- Set False Path from one clock to other ----------

set_property IOSTANDARD LVDS [get_ports DRP_CLK_IN_P]
set_property IOSTANDARD LVCMOS18 [get_ports TRACK_DATA_OUT]

set_property PACKAGE_PIN U2 [get_ports DRP_CLK_IN_P]
set_property PACKAGE_PIN R8 [get_ports TRACK_DATA_OUT]
set_property C_CLK_INPUT_FREQ_HZ 300000000 [get_debug_cores dbg_hub]
set_property C_ENABLE_CLK_DIVIDER false [get_debug_cores dbg_hub]
set_property C_USER_SCAN_CHAIN 1 [get_debug_cores dbg_hub]
connect_debug_port dbg_hub/clk [get_nets DRPCLK_IN]

#######################################################################
I got this error in the implementation, and I have no idea what is the reason:
ERROR: [Labtools 27-1395] Unable to arm ILA 'hw_ila_5'. The core clock is slow or no core clock connected for this ILA or the ILA core may not meet timing.
ERROR: [Xicom 50-38] xicom: Core access failed. Check cable connectivity and that the target board is powered up then use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target. Use open_hw_target to re-register the hardware device.

Please help.

--Huey

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    That error means that you do not have a clock running your debug logic.  The JTAG cannot communicate with whatever debug core you are trying to attach to. 

    What is your source clock that drives everything?  Are you using a block design to draw out the schematic?

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to drozwood90

    Hi Dan

    Please help.
    I instantiated the GTX 10GBASE-R example design to the processing wrapper. I am using the FCLK_CLK0 with 60Mhz in PS only for getting the clocks required for GTX: INIT_CLOCK_P and DRP_CLK_IN. And my top module like this:
    ################################################################
    `timescale 1 ps / 1 ps

    module design_1_wrapper
       (Q0_CLK1_GTREFCLK_PAD_N_IN,
        Q0_CLK1_GTREFCLK_PAD_P_IN,
        TRACK_DATA_OUT,
        RXN_IN,
        RXP_IN,
        TXN_OUT,
        TXP_OUT,
        DDR_addr,
        DDR_ba,
        DDR_cas_n,
        DDR_ck_n,
        DDR_ck_p,
        DDR_cke,
        DDR_cs_n,
        DDR_dm,
        DDR_dq,
        DDR_dqs_n,
        DDR_dqs_p,
        DDR_odt,
        DDR_ras_n,
        DDR_reset_n,
        DDR_we_n,
        FCLK_CLK0,
        FIXED_IO_ddr_vrn,
        FIXED_IO_ddr_vrp,
        FIXED_IO_mio,
        FIXED_IO_ps_clk,
        FIXED_IO_ps_porb,
        FIXED_IO_ps_srstb);
        input   Q0_CLK1_GTREFCLK_PAD_N_IN;
        input   Q0_CLK1_GTREFCLK_PAD_P_IN;
        (*mark_debug = "TRUE" *)output  TRACK_DATA_OUT;
        input   [3:0]   RXN_IN;
        input   [3:0]   RXP_IN;
        output  [3:0]   TXN_OUT;
        output  [3:0]   TXP_OUT;
        inout [14:0]DDR_addr;
        inout [2:0]DDR_ba;
        inout DDR_cas_n;
        inout DDR_ck_n;
        inout DDR_ck_p;
        inout DDR_cke;
        inout DDR_cs_n;
        inout [3:0]DDR_dm;
        inout [31:0]DDR_dq;
        inout [3:0]DDR_dqs_n;
        inout [3:0]DDR_dqs_p;
        inout DDR_odt;
        inout DDR_ras_n;
        inout DDR_reset_n;
        inout DDR_we_n;
        output FCLK_CLK0;
        inout FIXED_IO_ddr_vrn;
        inout FIXED_IO_ddr_vrp;
        inout [53:0]FIXED_IO_mio;
        inout FIXED_IO_ps_clk;
        inout FIXED_IO_ps_porb;
        inout FIXED_IO_ps_srstb;

        wire   Q0_CLK1_GTREFCLK_PAD_N_IN;
        wire   Q0_CLK1_GTREFCLK_PAD_P_IN;
        wire  TRACK_DATA_OUT;
        wire   [3:0]   RXN_IN;
        wire   [3:0]   RXP_IN;
        wire  [3:0]   TXN_OUT;
        wire  [3:0]   TXP_OUT;
        wire [14:0]DDR_addr;
        wire [2:0]DDR_ba;
        wire DDR_cas_n;
        wire DDR_ck_n;
        wire DDR_ck_p;
        wire DDR_cke;
        wire DDR_cs_n;
        wire [3:0]DDR_dm;
        wire [31:0]DDR_dq;
        wire [3:0]DDR_dqs_n;
        wire [3:0]DDR_dqs_p;
        wire DDR_odt;
        wire DDR_ras_n;
        wire DDR_reset_n;
        wire DDR_we_n;
        wire FCLK_CLK0;
        wire FIXED_IO_ddr_vrn;
        wire FIXED_IO_ddr_vrp;
        wire [53:0]FIXED_IO_mio;
        wire FIXED_IO_ps_clk;
        wire FIXED_IO_ps_porb;
        wire FIXED_IO_ps_srstb;

      design_1 design_1_i
           (.DDR_addr(DDR_addr),
            .DDR_ba(DDR_ba),
            .DDR_cas_n(DDR_cas_n),
            .DDR_ck_n(DDR_ck_n),
            .DDR_ck_p(DDR_ck_p),
            .DDR_cke(DDR_cke),
            .DDR_cs_n(DDR_cs_n),
            .DDR_dm(DDR_dm),
            .DDR_dq(DDR_dq),
            .DDR_dqs_n(DDR_dqs_n),
            .DDR_dqs_p(DDR_dqs_p),
            .DDR_odt(DDR_odt),
            .DDR_ras_n(DDR_ras_n),
            .DDR_reset_n(DDR_reset_n),
            .DDR_we_n(DDR_we_n),
            .FCLK_CLK0(FCLK_CLK0),
            .FIXED_IO_ddr_vrn(FIXED_IO_ddr_vrn),
            .FIXED_IO_ddr_vrp(FIXED_IO_ddr_vrp),
            .FIXED_IO_mio(FIXED_IO_mio),
            .FIXED_IO_ps_clk(FIXED_IO_ps_clk),
            .FIXED_IO_ps_porb(FIXED_IO_ps_porb),
            .FIXED_IO_ps_srstb(FIXED_IO_ps_srstb));
           
        gtwizard_0_exdes gtwizard0exdes
            (
                .Q0_CLK1_GTREFCLK_PAD_N_IN(Q0_CLK1_GTREFCLK_PAD_N_IN),
                .Q0_CLK1_GTREFCLK_PAD_P_IN(Q0_CLK1_GTREFCLK_PAD_P_IN),
                .DRP_CLK_IN_P(FCLK_CLK0),
                .DRP_CLK_IN_N(FCLK_CLK0),
                .TRACK_DATA_OUT(TRACK_DATA_OUT),
                .RXN_IN(RXN_IN),
                .RXP_IN(RXP_IN),
                .TXN_OUT(TXN_OUT),
                .TXP_OUT(TXP_OUT)
            );
    endmodule
    ###############################################

    I got the errors during DRC:
    Implementation
    Place Design
    [DRC 23-20] Rule violation (REQP-61) ibufds_connects_I_active - IBUFDS gtwizard0exdes/IBUFDS_DRP_CLK pin I has an invalid driver design_1_i/processing_system7_0/inst/buffer_fclk_clk_0.FCLK_CLK_0_BUFG

    [DRC 23-20] Rule violation (REQP-62) ibufds_connects_IB_active - IBUFDS gtwizard0exdes/IBUFDS_DRP_CLK pin IB has an invalid driver design_1_i/processing_system7_0/inst/buffer_fclk_clk_0.FCLK_CLK_0_BUFG

    [Vivado_Tcl 4-23] Error(s) found during DRC. Placer not run.

    Thanks.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to drozwood90

    Hi Dan

    Please help.
    I instantiated the GTX 10GBASE-R example design to the processing wrapper. I am using the FCLK_CLK0 with 60Mhz in PS only for getting the clocks required for GTX: INIT_CLOCK_P and DRP_CLK_IN. And my top module like this:
    ################################################################
    `timescale 1 ps / 1 ps

    module design_1_wrapper
       (Q0_CLK1_GTREFCLK_PAD_N_IN,
        Q0_CLK1_GTREFCLK_PAD_P_IN,
        TRACK_DATA_OUT,
        RXN_IN,
        RXP_IN,
        TXN_OUT,
        TXP_OUT,
        DDR_addr,
        DDR_ba,
        DDR_cas_n,
        DDR_ck_n,
        DDR_ck_p,
        DDR_cke,
        DDR_cs_n,
        DDR_dm,
        DDR_dq,
        DDR_dqs_n,
        DDR_dqs_p,
        DDR_odt,
        DDR_ras_n,
        DDR_reset_n,
        DDR_we_n,
        FCLK_CLK0,
        FIXED_IO_ddr_vrn,
        FIXED_IO_ddr_vrp,
        FIXED_IO_mio,
        FIXED_IO_ps_clk,
        FIXED_IO_ps_porb,
        FIXED_IO_ps_srstb);
        input   Q0_CLK1_GTREFCLK_PAD_N_IN;
        input   Q0_CLK1_GTREFCLK_PAD_P_IN;
        (*mark_debug = "TRUE" *)output  TRACK_DATA_OUT;
        input   [3:0]   RXN_IN;
        input   [3:0]   RXP_IN;
        output  [3:0]   TXN_OUT;
        output  [3:0]   TXP_OUT;
        inout [14:0]DDR_addr;
        inout [2:0]DDR_ba;
        inout DDR_cas_n;
        inout DDR_ck_n;
        inout DDR_ck_p;
        inout DDR_cke;
        inout DDR_cs_n;
        inout [3:0]DDR_dm;
        inout [31:0]DDR_dq;
        inout [3:0]DDR_dqs_n;
        inout [3:0]DDR_dqs_p;
        inout DDR_odt;
        inout DDR_ras_n;
        inout DDR_reset_n;
        inout DDR_we_n;
        output FCLK_CLK0;
        inout FIXED_IO_ddr_vrn;
        inout FIXED_IO_ddr_vrp;
        inout [53:0]FIXED_IO_mio;
        inout FIXED_IO_ps_clk;
        inout FIXED_IO_ps_porb;
        inout FIXED_IO_ps_srstb;

        wire   Q0_CLK1_GTREFCLK_PAD_N_IN;
        wire   Q0_CLK1_GTREFCLK_PAD_P_IN;
        wire  TRACK_DATA_OUT;
        wire   [3:0]   RXN_IN;
        wire   [3:0]   RXP_IN;
        wire  [3:0]   TXN_OUT;
        wire  [3:0]   TXP_OUT;
        wire [14:0]DDR_addr;
        wire [2:0]DDR_ba;
        wire DDR_cas_n;
        wire DDR_ck_n;
        wire DDR_ck_p;
        wire DDR_cke;
        wire DDR_cs_n;
        wire [3:0]DDR_dm;
        wire [31:0]DDR_dq;
        wire [3:0]DDR_dqs_n;
        wire [3:0]DDR_dqs_p;
        wire DDR_odt;
        wire DDR_ras_n;
        wire DDR_reset_n;
        wire DDR_we_n;
        wire FCLK_CLK0;
        wire FIXED_IO_ddr_vrn;
        wire FIXED_IO_ddr_vrp;
        wire [53:0]FIXED_IO_mio;
        wire FIXED_IO_ps_clk;
        wire FIXED_IO_ps_porb;
        wire FIXED_IO_ps_srstb;

      design_1 design_1_i
           (.DDR_addr(DDR_addr),
            .DDR_ba(DDR_ba),
            .DDR_cas_n(DDR_cas_n),
            .DDR_ck_n(DDR_ck_n),
            .DDR_ck_p(DDR_ck_p),
            .DDR_cke(DDR_cke),
            .DDR_cs_n(DDR_cs_n),
            .DDR_dm(DDR_dm),
            .DDR_dq(DDR_dq),
            .DDR_dqs_n(DDR_dqs_n),
            .DDR_dqs_p(DDR_dqs_p),
            .DDR_odt(DDR_odt),
            .DDR_ras_n(DDR_ras_n),
            .DDR_reset_n(DDR_reset_n),
            .DDR_we_n(DDR_we_n),
            .FCLK_CLK0(FCLK_CLK0),
            .FIXED_IO_ddr_vrn(FIXED_IO_ddr_vrn),
            .FIXED_IO_ddr_vrp(FIXED_IO_ddr_vrp),
            .FIXED_IO_mio(FIXED_IO_mio),
            .FIXED_IO_ps_clk(FIXED_IO_ps_clk),
            .FIXED_IO_ps_porb(FIXED_IO_ps_porb),
            .FIXED_IO_ps_srstb(FIXED_IO_ps_srstb));
           
        gtwizard_0_exdes gtwizard0exdes
            (
                .Q0_CLK1_GTREFCLK_PAD_N_IN(Q0_CLK1_GTREFCLK_PAD_N_IN),
                .Q0_CLK1_GTREFCLK_PAD_P_IN(Q0_CLK1_GTREFCLK_PAD_P_IN),
                .DRP_CLK_IN_P(FCLK_CLK0),
                .DRP_CLK_IN_N(FCLK_CLK0),
                .TRACK_DATA_OUT(TRACK_DATA_OUT),
                .RXN_IN(RXN_IN),
                .RXP_IN(RXP_IN),
                .TXN_OUT(TXN_OUT),
                .TXP_OUT(TXP_OUT)
            );
    endmodule
    ###############################################

    I got the errors during DRC:
    Implementation
    Place Design
    [DRC 23-20] Rule violation (REQP-61) ibufds_connects_I_active - IBUFDS gtwizard0exdes/IBUFDS_DRP_CLK pin I has an invalid driver design_1_i/processing_system7_0/inst/buffer_fclk_clk_0.FCLK_CLK_0_BUFG

    [DRC 23-20] Rule violation (REQP-62) ibufds_connects_IB_active - IBUFDS gtwizard0exdes/IBUFDS_DRP_CLK pin IB has an invalid driver design_1_i/processing_system7_0/inst/buffer_fclk_clk_0.FCLK_CLK_0_BUFG

    [Vivado_Tcl 4-23] Error(s) found during DRC. Placer not run.

    Thanks.