Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Software Controled Multiplexer of EMMC and MIO pins
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 336 subscribers
  • Views 955 views
  • Users 0 members are here
  • picozed
Related

Software Controled Multiplexer of EMMC and MIO pins

zeevmairav
zeevmairav over 5 years ago

i am using Picozed 7030. The bank 500 MIO pins (MIO 0 and 9-15) are multiplexed with the on-board EMMC device

There is a multiplexer between the two uses - MIO or EMMC - which is connected by default to MIO 0 so it can be activated by SW.

My intention is to use part of the pins as I2C, and use the EMMC only in boot time.

The question is, how do I tell the PS that there are two uses to the same pins.

In the "peripheral IO pins" page in Vivado only one use of each MIO pin is allowed.

If anyone has experience in utilizing this option and can explain how it is done it would be a great help.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 5 years ago

    The mux is only available on Rev C and earlier. See this post:

    https://www.element14.com/community/message/253922/l/emmc-fix-high-speed-but-remove-ps-mio-mux#253922

     

    You can still purchase the Rev C, but it has to be done by special order with a minimum order quantity of 100 since it is build to order.

     

    Are you able to use the I2C through EMIO on some of the PL IOs?

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • zeevmairav
    0 zeevmairav over 5 years ago in reply to bhfletcher

    Hi Brian,

     

    Thanks for the prompt reply

    Following your reply I decided to make two wire modifications to the board and connect the I2C to spare EMIO pins I have instead of those MIO pins

    I am currently working with picozed version C and I have a few of those, but for future sake I cannot rely on that.

     

    Thanks

     

    Zeev

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zeevmairav
    0 zeevmairav over 5 years ago in reply to bhfletcher

    Hi Brian,

     

    Thanks for the prompt reply

    Following your reply I decided to make two wire modifications to the board and connect the I2C to spare EMIO pins I have instead of those MIO pins

    I am currently working with picozed version C and I have a few of those, but for future sake I cannot rely on that.

     

    Thanks

     

    Zeev

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bhfletcher
    0 bhfletcher over 5 years ago in reply to zeevmairav

    Zeev,

     

    I think that is the best way to go. Using the PS I2C through EMIO to a PL IO is a great alternative. Plus, with Rev E PicoZed, you will get more reliable performance of the eMMC across the full temperature range. That mux was a good idea in the beginning, but it just added too much timing uncertainty which resulted in the cold failures we saw previously.

     

    Good luck!

    Bryan