Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Issue: PicoZED fmc Carrier V2 USB UART
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 1735 views
  • Users 0 members are here
  • picozed 7030
  • zedboardcmty
  • picozed fmc carrier card
Related

Issue: PicoZED fmc Carrier V2 USB UART

shreyasborse
shreyasborse over 6 years ago

Hello ,

I am using Picozed SOM 7030 and FMC carrier v2 and booting petalinux application using SDcard, but i can connect it using USB-UART to monitor on serial terminal.

I tried installing CP210X drivers for UBUNTU 16.04 it didn't work.

I installed it on WIN 7 x64 system too , but the COM port is not seen on the device manager.

Are there any hardware settings other than SW1 JP-5 , is there any other setting that can solve this problem kindly suggest! also if any other way to connect please suggest.

 

Thank You.

  • Sign in to reply
  • Cancel

Top Replies

  • bhfletcher
    bhfletcher over 6 years ago +1
    Does your system boot and configure the PL according to the DONE LED? Please confirm you are plugged into the microUSB J1 port. Do you see any LED change when you plug in the cable? Are you certain that…
  • narrucmot
    narrucmot over 6 years ago +1 verified
    Do you have a USB cable connected from J1 on the FMC2 carrier to your host PC? Does the blue FPGA DONE LED (D3) illuminate after turning on the board? Does the PS LED D10 blink? Are you running Ubuntu…
  • bhfletcher
    0 bhfletcher over 6 years ago

    Does your system boot and configure the PL according to the DONE LED?

     

    Please confirm you are plugged into the microUSB J1 port. Do you see any LED change when you plug in the cable?

     

    Are you certain that you installed the correct version of the drivers for your version of Windows?

    https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers

     

     

     

    Bryan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • narrucmot
    0 narrucmot over 6 years ago

    Do you have a USB cable connected from J1 on the FMC2 carrier to your host PC?

     

    Does the blue FPGA DONE LED (D3) illuminate after turning on the board? 

     

    Does the PS LED D10 blink?

     

    Are you running Ubuntu v16.04 native or in a virtual machine?  If in a virtual machine, is the Silicon Labs CP2104 device selected for use in the VM?  For VirtualBox this setting looks like this screenshot:

    image

     

    Does Ubuntu recognize that the USB UART device is present?  A simple way to check this is filter the Linux 'ls' command through 'grep' to search for the enumerated UAB UART devices:

    $ ls /dev | grep USB

    image

    Do you have the serial port settings correct?  They should be 115200,no parity,8 bits, 1 stop bit (115200,n,8,1).

     

    Is the PicoZed SOM fully seated in the JX connectors?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • shreyasborse
    0 shreyasborse over 6 years ago in reply to bhfletcher

    Yes it worked with WIN10 x64 MACHINE ;

    Thank you !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shreyasborse
    0 shreyasborse over 6 years ago in reply to narrucmot

    yes, i am using 16.04 no VM , finally i installed the drivers on win 10 system.

    its able to monitor throught USB UART,

    Although i will try install and using ls / dev

    Thanks alot!