Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Zynq Z7020 on picozed fried during SW download
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 358 subscribers
  • Views 1978 views
  • Users 0 members are here
  • dead chip
  • soc
  • zynq 7000
  • avnet
  • xilinx
  • picozed
Related

Zynq Z7020 on picozed fried during SW download

mashedcorn
mashedcorn over 3 years ago
I purchased a picozed 7Z20 and made a custom carrier board for it.  I was able to power it on and get the FPGA DONE LED to light up, I was able to program the Zynq chip PL through VIVADO, and I was able to begin programming the PS through vitis.  towards the end of downloading my SW to the board I lost JTAG connection and I am afraid my Z720 chip is now dead, it gets instantly hot when powered on and draws around 3x the current it did when I first booted it up. 
 
the board had been on for a fair amount of time, 10 minutes of power cycling it while trying to get it set up on a test bench, probably 5 minutes of me setting up and downloading the PL firmware a couple of times, 20 minutes between then and trying the SW download.
 
I'm wondering if anyone might have any insight into what went wrong here, Is it possible for the chip to overheat and kill itself?, I don't have any heatsink or fan on the chip but I figured there was some built in thermal protection but maybe I'm wrong.  Otherwise, I'm not sure what might have happened if it was working fine. I doubt JTAG programming could fry the chip
  • Sign in to reply
  • Cancel
Parents
  • flyingbean
    0 flyingbean over 3 years ago

    Here is a quick answer for Zynq FPGA power rails. The power rail table was from TI design for Zyqn 7015(tidua66.pdf):

    image

    Zynq 7015 is similar to 7020 except the high speed bus at PS side.

    One tip to check whether the FPGA is dead or not if you cannot use JTAG: check FPGA temperature after powering it on. If FPGA temperature is blow 40~50C after power on and the PS does have proper clock input/power rails are fine, FPGA most likely is dead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • flyingbean
    0 flyingbean over 3 years ago

    Here is a quick answer for Zynq FPGA power rails. The power rail table was from TI design for Zyqn 7015(tidua66.pdf):

    image

    Zynq 7015 is similar to 7020 except the high speed bus at PS side.

    One tip to check whether the FPGA is dead or not if you cannot use JTAG: check FPGA temperature after powering it on. If FPGA temperature is blow 40~50C after power on and the PS does have proper clock input/power rails are fine, FPGA most likely is dead.