Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio HDMI problem of PicoZed SDR FMC Carrier Card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 810 views
  • Users 0 members are here
Related

HDMI problem of PicoZed SDR FMC Carrier Card

e14 Contributor
e14 Contributor over 10 years ago

Hello,

We have a PicoZed Development Kit and every time we connect the HDMI cable the DS1 (in the PicoZed SDR FMC Carrier Card) is switch on and no image is shown in the Monitor.

The leds that are on are:

DS1
DS8
DS3
D3 (SOM)
D4 (SOM)

When we remove the HDMI cable the DS1 goes off. Is there any document about the leds functinallity and any recommend about what should we do?

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    Hello,

    Desktop Linux will often go to a power save mode and blank the screen.  We mostly notice this upon boot.  Have you tried shaking the mouse a little?  Is the HDMI cable connected at power on, or afterwards?

     

    We're working on the User's Guide for the FMC Carrier.  Meanwhile I can answer your question about the LEDS:

    DS1 : HDMI connected
    DS8 : FMC Carrier 5.0V regulator good
    DS3 - DS6 : GPIO LEDs
    D3 (SOM) : PG_MODULE (lights when SOM power supplies are good)
    D4 (SOM) :  FPGA_DONE (goes OFF when Zynq PL is configured)

     

    Thanks,
    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 10 years ago

    Hello,

    Desktop Linux will often go to a power save mode and blank the screen.  We mostly notice this upon boot.  Have you tried shaking the mouse a little?  Is the HDMI cable connected at power on, or afterwards?

     

    We're working on the User's Guide for the FMC Carrier.  Meanwhile I can answer your question about the LEDS:

    DS1 : HDMI connected
    DS8 : FMC Carrier 5.0V regulator good
    DS3 - DS6 : GPIO LEDs
    D3 (SOM) : PG_MODULE (lights when SOM power supplies are good)
    D4 (SOM) :  FPGA_DONE (goes OFF when Zynq PL is configured)

     

    Thanks,
    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Hello Matt,

    I used a USB HUB in order to connect mouse and keyboard in the USB OTG. The hub has itself a LED which never turned on. It looks like the usb port have no power at all. So, probably there are even more problems like that the USB port is not working at all.

    We had connected the HDMI when we started the device. We had waited for more than 45 secs and then we removed the HDMI cable, when we noticed that DS1 goes off.

    We had try also to connect to the device with the Ethernet cable but the devices had never assigned a IP address (checked many times with our IT manager, there was never a request to the router by the device).

    So finally, the device looks like it switch on the LEDs I wrote in my first message and stops there. Never boot or starts anything.

    Regards,

    Ilias