Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio PicoZed SDR Not Powering on 5V Only Custom Carrier
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 755 views
  • Users 0 members are here
Related

PicoZed SDR Not Powering on 5V Only Custom Carrier

e14 Contributor
e14 Contributor over 10 years ago

Trying to make a bare minimum PicoZed SDR Carrier card.  Designed a card that only provides the 5V rail, (according to the user guide should work):

 

4.16.1 Input Voltages

 

PicoZed SDR Z7035/AD9361 is powered from the carrier card through micro headers JX1, JX2, and JX3. There are six unique voltages that can be supplied to the module. The only mandatory input is the 5.0V system supply. The others are powered only as needed by your design.

 

My PicoZed SDR doesn't power up on the custom carrier (works fine on supplied carrier), I measured and the super sequencer is shutting down the board at Q13.

 

Looking at: https://wiki.analog.com/resources/eval/user-guides/pzsdr/power-and-sequencing

 

It seems like the super sequencer checks for JX_VCCO_12 JX_VCCO_13 JX_VCCO_33_34 JX_MGTAVTT JX_MGTAVCC, and if all of these are not present, goes into shutdown.

 

Seems like this conflicts with the non-mandatory statement in the user guide!

 

My question is can I salvage this carrier by reprogramming the ADM1166 to skip checking these rails, or is there a reason the ADM1166 is programmed to make them mandatory?

 

Thanks,

Jeremy

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Modified the ADM1166 firmware to remove the extra checks, and the SOM boots no problem!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Modified the ADM1166 firmware to remove the extra checks, and the SOM boots no problem!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer