Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Driving external clock to AD9361 (improper termination?)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Subscribers 361 subscribers
  • Views 2939 views
  • Users 0 members are here
Related

Driving external clock to AD9361 (improper termination?)

e14 Contributor
e14 Contributor over 10 years ago

Hi,

 

I'm making a custom carrier for the PicoZed SDR, which will connect an external clock to the AD9361.  Looking at the clock input circuit in the SOM schematics (pg. 8), I'm unsure what the proper way is to drive this.  The AD9361 datasheet says it wants a max 1.3Vpp clock, AC coupled.  It looks like when using the internal oscillator, it uses a capacitive divider with a series 18pF and using the ~7pF "on" capacitance of the switch and the ~10pF capacitance of the AD9361 input to drop the 1.8V oscillator down to ~0.9Vpp.

 

But for the external input, there's a 50 ohm termination resistor, and no AC coupling capacitor after it.  How do you recommend driving this?  Should that resistor (R5) be removed, and use a capacitive divider for my external clock?  If I provide an AC coupled signal that can drive 50 ohms, I believe the signal will be clipped by swinging below the rail of the switch (U5), and the resistor will also provide a 50 ohm DC path to ground from the XTALN input.

 

I also see that the development kit terminates at the SMA with 50 ohms and no AC coupling capacitor... which is essentially in parallel with the existing 50 ohms, making the clock input 25 ohm terminated when mated to the development kit.

 

Am I missing something, or is this an error that should be changed on a future rev?  And if so, what change would you expect to make?  Of course I'd like to design my carrier to be compatible with future revs without requiring additional modifications.

 

Thanks,
Pat

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    hi Matt,

     

    From the diagram, when IO_00_34_AD9361_CLKSEL is high, the external clock is selected but Y4 will also be enabled. Is this interpretation correct?

    Thanks!

    Tan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    hi Matt,

     

    From the diagram, when IO_00_34_AD9361_CLKSEL is high, the external clock is selected but Y4 will also be enabled. Is this interpretation correct?

    Thanks!

    Tan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mbrown
    0 mbrown over 9 years ago in reply to e14 Contributor

    Hi Tan:

    When IO_00_34_AD9361_CLKSEL is high, the 40MHz osc (Y4) is enabled; so is the MOSFET (Q6) which inverts the logic to the analog mux (U5) select pin IN1. This disables the S1A input and selects S1B which is connected to Y4.

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhatt_vinay1
    0 bhatt_vinay1 over 9 years ago in reply to mbrown

    In picozed sdr kit I am getting 40 MHz output clock at y4 output. Is io_00_34__ad9361_clksel default value is high? How fpga is giving high at this pin?  How  can I configure clock out from ad9361 to fpga?