Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio HDMI is not connected
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 26 replies
  • Subscribers 359 subscribers
  • Views 3275 views
  • Users 0 members are here
Related

HDMI is not connected

e14 Contributor
e14 Contributor over 10 years ago

Hi everyone! 

 

I have a PicoZed Development Kit and when I connect the HDMI cable the DS1 is not switch on. Other LEDs are switch good.

 

The leds that are on are:

DS8 (power) - red;

DS7 - blue;

D3 (SOM) - green;

D4 (SOM) is switch off, so Zynq PL is configured.

 

I'm connecting a monitor (VGA) through HDMI-VGA adapter. 

 

What could be the problem?

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    Now that you have re-imaged the SD card according to ADI wiki page, can you please confirm that you've followed the Quick Start instructions for the kit?

    http://picozed.org/sites/default/files/documentations/QSC-Kit%20-%20PicoZed%E2%84%A2%20SDR%20AD9361-v9.pdf

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Yes I followed the Quick Start Card. There are devices that are connected to the my board:

    1.   UART cable. I'm using Tera Term terminal on my Windows host but PC don't see virtual COM port from the board any more.
    2.   USB-microUSB adapter is connected to USB OTG on the board. I connect USB keyboard through this adapter.
    3.   Monitor is connected to HDMI on the board through HDMI-VGA adapter.
    4.   LTE/MIMO antenna using the included U.FL-to-SMA cables.
    5.   12V Power.
    6.   Ethernet cable from board to PC
    7.   S1, S3 and S4 on the SOM to the logical 1.
    8.   P8 on the FMC to 3.3V (I tried 2.5V and 1.8V, don't work)
    9.   P17 on the FMC to USB OTG.

    I remind that only the DS8 (5V power) led turn on after that I turn on the board. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Yes I followed the Quick Start Card. There are devices that are connected to the my board:

    1.   UART cable. I'm using Tera Term terminal on my Windows host but PC don't see virtual COM port from the board any more.
    2.   USB-microUSB adapter is connected to USB OTG on the board. I connect USB keyboard through this adapter.
    3.   Monitor is connected to HDMI on the board through HDMI-VGA adapter.
    4.   LTE/MIMO antenna using the included U.FL-to-SMA cables.
    5.   12V Power.
    6.   Ethernet cable from board to PC
    7.   S1, S3 and S4 on the SOM to the logical 1.
    8.   P8 on the FMC to 3.3V (I tried 2.5V and 1.8V, don't work)
    9.   P17 on the FMC to USB OTG.

    I remind that only the DS8 (5V power) led turn on after that I turn on the board.