Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio HDMI is not connected
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 26 replies
  • Subscribers 359 subscribers
  • Views 3282 views
  • Users 0 members are here
Related

HDMI is not connected

e14 Contributor
e14 Contributor over 10 years ago

Hi everyone! 

 

I have a PicoZed Development Kit and when I connect the HDMI cable the DS1 is not switch on. Other LEDs are switch good.

 

The leds that are on are:

DS8 (power) - red;

DS7 - blue;

D3 (SOM) - green;

D4 (SOM) is switch off, so Zynq PL is configured.

 

I'm connecting a monitor (VGA) through HDMI-VGA adapter. 

 

What could be the problem?

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    Initially, you were able to power up and power the SOM:

    DS8 (power) - red;
    DS7 - blue;
    D3 (SOM) - green;
    D4 (SOM) is switch off, so Zynq PL is configured.

     

    But now, you don't even see D3 (SOM) light up, indicating that it's not powering up successfully.

     

    Is that correct?

     

    P8 position should not matter. Are you saying that when Vadj is set for 3.3V the system powers up? (D3 SOM illuminates?)

     

    Thanks for clarifying. I want to make sure we debug first things first.

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Something else when booting linux:

     

    " * Setting up X directories...  [OK]

       * STARTDISTCC is set to false in /etc/default/distcc

       * /usr/bin/distcc not starting

       * Starting IIO Daemon iiod   [OK]"

     

    As I know this problem may be in "STARTDISTCC" then not started. 

    The rest of the Linux boot normally but only through the terminal to the PC. Monitor in not working. VGA-HDMI adapter may be the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Something else when booting linux:

     

    " * Setting up X directories...  [OK]

       * STARTDISTCC is set to false in /etc/default/distcc

       * /usr/bin/distcc not starting

       * Starting IIO Daemon iiod   [OK]"

     

    As I know this problem may be in "STARTDISTCC" then not started. 

    The rest of the Linux boot normally but only through the terminal to the PC. Monitor in not working. VGA-HDMI adapter may be the problem.