Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio PicoZed Questions
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 360 subscribers
  • Views 1764 views
  • Users 0 members are here
Related

PicoZed Questions

e14 Contributor
e14 Contributor over 10 years ago

We plan on using the PicoZed kit:

http://www.xilinx.com/products/boards-and-kits/1-au200Bskjht.html



1) It shows that the band is 70MHz to 6GHz.  We were wondering if the kit is ever run up to 6GHz or rather, is it practical.  What's the typical operating range?  



2) I got the user's manual 1.2 and near the end it states that the datasheet uses narrowband baluns while the test uses wideband baluns for the PicoZed SDR Z7035/AD9361.  Is it confirmed that this model uses wideband baluns (or both)?



3) Where can we find a footprint of the chip?  I don't think the manual has a clear one.



Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 8 years ago +1
    Hello, 1. For the PicoZed SOM, the only Carrier Card we hvae available that oprates with it is the PicoZed FMC V2. However, this does not prevent you from making your own custom carrier card. The PicoZed…
Parents
  • mbrown
    0 mbrown over 10 years ago

    Yes it is practical to run the module over the same range as the spec for the AD9361, which is 70MHz to 6GHz.  Special attention was paid to board layout, shielding, etc. to ensure that the module contributed very little signal degradation.  That's why you see the EVM test in the User Guide run over the entire range.

     

    The PicoZed SDR Z7035/AD9361 SOM uses wideband baluns.  We expect that your custom carrier will implement selective filtering for your carrier band of interest.

     

    Which chip footprint do you want, the AD9361 footprint?  Analog Devices website.

     

    Thanks,

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 10 years ago

    Yes it is practical to run the module over the same range as the spec for the AD9361, which is 70MHz to 6GHz.  Special attention was paid to board layout, shielding, etc. to ensure that the module contributed very little signal degradation.  That's why you see the EVM test in the User Guide run over the entire range.

     

    The PicoZed SDR Z7035/AD9361 SOM uses wideband baluns.  We expect that your custom carrier will implement selective filtering for your carrier band of interest.

     

    Which chip footprint do you want, the AD9361 footprint?  Analog Devices website.

     

    Thanks,

    /Matt