Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio PicoZed Questions
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 360 subscribers
  • Views 1764 views
  • Users 0 members are here
Related

PicoZed Questions

e14 Contributor
e14 Contributor over 10 years ago

We plan on using the PicoZed kit:

http://www.xilinx.com/products/boards-and-kits/1-au200Bskjht.html



1) It shows that the band is 70MHz to 6GHz.  We were wondering if the kit is ever run up to 6GHz or rather, is it practical.  What's the typical operating range?  



2) I got the user's manual 1.2 and near the end it states that the datasheet uses narrowband baluns while the test uses wideband baluns for the PicoZed SDR Z7035/AD9361.  Is it confirmed that this model uses wideband baluns (or both)?



3) Where can we find a footprint of the chip?  I don't think the manual has a clear one.



Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 8 years ago +1
    Hello, 1. For the PicoZed SOM, the only Carrier Card we hvae available that oprates with it is the PicoZed FMC V2. However, this does not prevent you from making your own custom carrier card. The PicoZed…
Parents
  • thammire
    0 thammire over 8 years ago

    Hi, Will someone help me questions related to picozed board,

    1.  Will you please tell me if carrier card is compulsory to work with picozed card?

    2.  how many user programmable switches and LEDs are available on the picozed board?

    3. In the possible application areas for zedboard, its mentioned on the avnet website that, it can be used for "General Zynq-7000 All Programmable SoC prototyping". The same application is missing in picozed description. I am really worried that, if I buy picozed, can't I use picozed for general prototyping?
     
      
        4. Zedboards has user programmable LEDs,and switches. The similar ones seems to be missing in picozed. How to program picozed for applying inputs in real time from switches and observing LEDs from output?
       
        5. Difference between  system on module(SoM) and system on chip(SoC)
     
     

    6. Can I use XADC in picozed without any issues?

      Sorry, if I ask novice questions.

    Thanks.

    thammire

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • thammire
    0 thammire over 8 years ago

    Hi, Will someone help me questions related to picozed board,

    1.  Will you please tell me if carrier card is compulsory to work with picozed card?

    2.  how many user programmable switches and LEDs are available on the picozed board?

    3. In the possible application areas for zedboard, its mentioned on the avnet website that, it can be used for "General Zynq-7000 All Programmable SoC prototyping". The same application is missing in picozed description. I am really worried that, if I buy picozed, can't I use picozed for general prototyping?
     
      
        4. Zedboards has user programmable LEDs,and switches. The similar ones seems to be missing in picozed. How to program picozed for applying inputs in real time from switches and observing LEDs from output?
       
        5. Difference between  system on module(SoM) and system on chip(SoC)
     
     

    6. Can I use XADC in picozed without any issues?

      Sorry, if I ask novice questions.

    Thanks.

    thammire