Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Picozed SDR Development Board not powering up
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 43 replies
  • Subscribers 359 subscribers
  • Views 3999 views
  • Users 0 members are here
Related

Picozed SDR Development Board not powering up

e14 Contributor
e14 Contributor over 10 years ago

Hi there
I have just received my Picozed SDR SOM Development Kit. I have followed the quick start guide but the SOM is simply not powering up. Only one red LED DS8 turns on when i switch the board on and then nothing further. Plz help guys it is urgent. Thnx in advance

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    Gentlemen,

     

    Sorry to hear you're having trouble.  We're working on understanding this issue today.

    DS8 on the PZSDRCC-FMC board indicates that it is successfully generates 5.0V, which is used to power the SOM (VIN).

    Each PZSDRCC-FMC board is tested at the manufacturer, so I don't suspect you have bad carrier cards. 

    Our theory is that the firmware in the ADM1166 located on the AES-7ZPZ-SDR2-G SOM is programmed with a threshold for the VIN voltage that is too tight.  If the ADM1166 doesn't see a valid VIN voltage, the SOM will not power up.  We suspect this is what you are experiencing.

     

    We'll continue working on it and I will provide an update first thing in the morning.

     

    Thanks,

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 10 years ago

    Gentlemen,

     

    Sorry to hear you're having trouble.  We're working on understanding this issue today.

    DS8 on the PZSDRCC-FMC board indicates that it is successfully generates 5.0V, which is used to power the SOM (VIN).

    Each PZSDRCC-FMC board is tested at the manufacturer, so I don't suspect you have bad carrier cards. 

    Our theory is that the firmware in the ADM1166 located on the AES-7ZPZ-SDR2-G SOM is programmed with a threshold for the VIN voltage that is too tight.  If the ADM1166 doesn't see a valid VIN voltage, the SOM will not power up.  We suspect this is what you are experiencing.

     

    We'll continue working on it and I will provide an update first thing in the morning.

     

    Thanks,

    /Matt