Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Picozed SDR Development Board not powering up
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 43 replies
  • Subscribers 359 subscribers
  • Views 3999 views
  • Users 0 members are here
Related

Picozed SDR Development Board not powering up

e14 Contributor
e14 Contributor over 10 years ago

Hi there
I have just received my Picozed SDR SOM Development Kit. I have followed the quick start guide but the SOM is simply not powering up. Only one red LED DS8 turns on when i switch the board on and then nothing further. Plz help guys it is urgent. Thnx in advance

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    i also have the same theory because TP2 on the SOM is reading 4.96V but power good led DS3 on SOM is not lighting up indicating that power supervisory IC is not completing its sequence. plz help me with this issue i am looking for a solution urgently. do i have to RMA the board ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mbrown
    0 mbrown over 10 years ago in reply to e14 Contributor

    We found the root cause.  It is *not* faulty hardware. 

     

    As we suspected, the threshold check of the voltage "VH" programmed into the ADM1166 (power sequencer) on the SOM was too tight.  VH is the first check performed by the ADM1166.  Therefore on some hardware combinations the SOM doesn't power up because the VIN voltage falls below the threshold (only by 10mV or so).

     

    The ADM1166 I2C lines connect directly to the Zynq device and therefore can be reprogrammed from software.  We are working on that software now and will publish it ASAP (target =Monday 2/29 ).

     

    Thank you for your patience and sorry for the inconvenience. 

     

    Farhan -- I will contact you via private message to see if you need an interim fix today.

     

    Thanks,

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 10 years ago in reply to e14 Contributor

    We found the root cause.  It is *not* faulty hardware. 

     

    As we suspected, the threshold check of the voltage "VH" programmed into the ADM1166 (power sequencer) on the SOM was too tight.  VH is the first check performed by the ADM1166.  Therefore on some hardware combinations the SOM doesn't power up because the VIN voltage falls below the threshold (only by 10mV or so).

     

    The ADM1166 I2C lines connect directly to the Zynq device and therefore can be reprogrammed from software.  We are working on that software now and will publish it ASAP (target =Monday 2/29 ).

     

    Thank you for your patience and sorry for the inconvenience. 

     

    Farhan -- I will contact you via private message to see if you need an interim fix today.

     

    Thanks,

    Matt