Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Can't connect Matlab to PicoZed SDR
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 821 views
  • Users 0 members are here
Related

Can't connect Matlab to PicoZed SDR

e14 Contributor
e14 Contributor over 10 years ago

I'm able to ping Picozed from Terminal on Linux laptop.

PicoZed is on 192.168.3.2
Laptop is on 192.168.3.3

Then I start MATLAB on Linux laptop.  I follow instructions in Matlab documentation  for "Manual Host-Radio Hardware Setup".  In "Step 3", I successfully do:
dev = sdrdev('PicoZed SDR');
setupSession(dev);

Then, I go to "Step 8" and get a warning and error when I do:
i = info(dev)

And I also get an error when I do:
setAddress(dev, 'IP Address', '192.168.3.2');

I tried to upload a Matlab screenshot to:

http://picozed.org/imce?app=ckeditor%7Csendto%40ckeditor_imceSendTo%7C&CKEditor=edit-body-und-0-value&CKEditorFuncNum=2&langCode=en

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    Hi Jeff,

    Which Linux image are you booting Zynq with? Is it the ADI image that came with the SD card, or did you update to the MathWorks Linux image, which is required in order to do streaming with Matlab & Simulink.

     

    See this post for more info -- http://picozed.org/content/sd-card-image-picozed-sdr

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Hi Matt,

    I was not using the Mathworks image.  I am now, and it works!  Thanks!  --Jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Hi Matt,

    I was not using the Mathworks image.  I am now, and it works!  Thanks!  --Jeff