Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
RFSoC Boards CLK104 PLL Lock
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 3138 views
  • Users 0 members are here
Related

CLK104 PLL Lock

dchien
dchien over 3 years ago

The CLK104 clock board on my ZCU208 evaluation board does not have all PLL lock LEDs on. The clock distribution PLL (U2) has its lock LED (DS1) on, but the DAC PLL (U7) has its LED (DS3) off and the ADC PLL (U5) has its lock LED (DS2) off. Do I have a defective CLK104 board? What can cause the ADC and DAC PLLs not locking (LEDs off)?

Thanks!image

  • Sign in to reply
  • Cancel

Top Replies

  • lightcollector
    lightcollector over 3 years ago in reply to dchien +1
    Hi, That tool does not provide any direct way to re-program the CLK104. So do you have a need to reprogram the CLK104 or are you just trying to use the defaults here? And are you just trying to rearrange…
Parents
  • lightcollector
    lightcollector over 3 years ago

    Hi,

    The clock 104 board is programmable using PS oriented software.  Can you please clarify which software you are running on the zcu208 and, or, what remote control PC program to configure the zcu208?  And also please, what are you trying to have the clk104 do?

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dchien
    dchien over 3 years ago in reply to lightcollector

    I am using https://github.com/AvnetDev/hdlcoder-zcu208-zip/releases/tag/v1.03 SD image with MATLAB HDL Coder design flow to implement signal processing with ADC running at 2GSPS and DAC running at 6GSPS. Thannks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dchien
    dchien over 3 years ago in reply to lightcollector

    I am using https://github.com/AvnetDev/hdlcoder-zcu208-zip/releases/tag/v1.03 SD image with MATLAB HDL Coder design flow to implement signal processing with ADC running at 2GSPS and DAC running at 6GSPS. Thannks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • lightcollector
    lightcollector over 3 years ago in reply to dchien

    Hi, That tool does not provide any direct way to re-program the CLK104. So do you have a need to reprogram the CLK104 or are you just trying to use the defaults here?  And are you just trying to rearrange the clock distirbution internally using the options that HDL Coder provides?

    One tip I can offer is that if you have generated the Vivado project using HDL Coder, you can open the design directly in Vivado and inspect the RF Data Converter IP.  Specifically inspect the clock distribution properties tab to make sure it is happy with the settings you selected.

    A sort of funny thing here is that mbrown had my board to start with, so I don't have a board either to double check the LEDs at this time.  Sorry about that, just wanted to clear that up as to why I can't firsthand verify your direct question.

    Understanding your intentions about what you are trying to accomplish with the system clock distribution would help provide better guidance or alternative solutions.

    We do work with MathWorks and I believe we will be having a direct meeting sometime soon.  If you want to converse directly before that, you can send an email to: rfinfo @ Avnet DOT com  mention you want to speak with LightCollector and the person that manages that email will forward me your email and we can converse directly if you would like.

    Thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dchien
    dchien over 3 years ago in reply to lightcollector

    Hi, I am using the default clock configuration from the HDL Coder design flow within MATLAB. I had a working ZCU208 setup also and did not pay attention to the two ADC/DAC PLL lock LED status at the time. I am working on a second setup and the first setup is not with me anymore. I am experiencing issues with my design that works at lower IF but fails at higher IF. Then I notice the PLL lock LEDs not on. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lightcollector
    lightcollector over 3 years ago in reply to dchien

    Ha, none of us seem to be able to hang onto our zcu208 boards :-)

    Would have to have more details to determine why a higher IF mixer frequency is impacting your progress.  There are many reasons why higher IF frequencies could have issues.  Not sure what your system level understanding is, but one possible explanation is that without IMR DAC mode turned on, 2 images come out the DAC.  If you don't have proper low or bandpass filtering in the analog domain, it can result in aliasing in your ADC samples.  Again, if you want to have a more detailed discussion reach out to the address I sent.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dchien
    dchien over 3 years ago in reply to lightcollector

    I have a bandpass filter on the IF input to the ADC. The high and low IF issue is on the input ADC side. I sent an email to the address you specified at 1:21pm Pacific. Hope to connect with you soon. Thanks.