Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
RFSoC Boards RFSoC ZCU208 HDL Coder Support in MATLAB/Simulink
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • +1 person also asked this people also asked this
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 349 subscribers
  • Views 4087 views
  • Users 0 members are here
  • zcu208
  • zcu111
  • ZCU216
  • hdl coder
  • rfsoc
Related

RFSoC ZCU208 HDL Coder Support in MATLAB/Simulink

jgabaldo55
jgabaldo55 over 2 years ago

I have an RFSoC ZCU208 board.  I went through the example found here:

Getting started with HDL Coder for the Xilinx ZCU208 RFSoC Gen 3 development board — hdlcoder-docs v1.0.0 documentation (rfsoc-hdlcoder.readthedocs.io)

I was able to successfully complete steps 1 - 10 and program the fpga with the example bitstream (from the adcdemo example) generated from the attached MATLAB/Simulink files.  I then proceeded to try and rebuild the adcdemo example using the "HDL Workflow Advisor" in Simulink so that I can see the process from start to finish.  While in the tool, on the step "Set Target Device and Synthesis Tool", I set "Target Workflow" to "IP Core Generation" but when I went to set "Target Platform", it did not give me the option for "Xilinx Zynq Ultrascale+ RFSoC ZCU208 Evaluation Board" like it does in the example.  I am wondering why that is.  The only boards that are available of the "Xilinx Zynq Ultrascale+ RFSoC" type are the ZCU111 and ZCU216.

Has anyone else experienced this?  I am wondering if the ZCU208 support was removed from the Support Packages for whatever reason?  I downloaded the correct support packages, which include the "HDL Coder Support Package for Xilinx RFSoC Devices" and the "HDL Coder Support Package for Zynq."  If anyone has any suggestions or insights, it would be greatly appreciated.

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • lightcollector
    lightcollector over 2 years ago +2
    Hi there, not sure but the zcu208 plug in code is partly installed with RFSoC Explorer, then you need to run the install m file (included in the extra zcu208 zip file per the instructions), which adds…
  • lightcollector
    lightcollector over 2 years ago in reply to jgabaldo55 +2 suggested
    Hi, Thanks for the info, I have a theory now why it is not working for you. By the way, MathWorks does not directly support the ZCU208 board, that is correct. However MathWorks does authorize Avnet to…
  • lightcollector
    lightcollector over 2 years ago in reply to jgabaldo55 +2
    Glad you were able to get it working. Regarding using a different version of Vivado, this is not feasible for the RFSoC development boards and these MathWorks tools. One reason is that the tcl code for…
Parents
  • forche
    +1 forche over 1 year ago

    I had the same issue and I was able to solve that. I am also using Matlab R2023b version.

    First you have to install Avnet RFSoC Explorer latest version from chrome (download it as Toolbox) and from Matlab access the toolbox, double click and install. After that if you navigate to Matlab Add-ons folder from file explorer, MATLAB Add-Ons>Toolboxes>Avnet RFSoC Explorer Toolbox>avnet_hdlcoder>zcu208, there you can find +ZCU208 add that to ProgramData> MATLAB> SupportPackages> R2022b> toolbox> shared> supportpackages> rfsoc_shared> boards> +ZynqRFSoC where you can find other RFSoC devices. If MATLAB is already open close it and reopen. Then you can find ZCU208 device listed in Target Platform selection.

    Hope it helps, it worked for me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • forche
    +1 forche over 1 year ago

    I had the same issue and I was able to solve that. I am also using Matlab R2023b version.

    First you have to install Avnet RFSoC Explorer latest version from chrome (download it as Toolbox) and from Matlab access the toolbox, double click and install. After that if you navigate to Matlab Add-ons folder from file explorer, MATLAB Add-Ons>Toolboxes>Avnet RFSoC Explorer Toolbox>avnet_hdlcoder>zcu208, there you can find +ZCU208 add that to ProgramData> MATLAB> SupportPackages> R2022b> toolbox> shared> supportpackages> rfsoc_shared> boards> +ZynqRFSoC where you can find other RFSoC devices. If MATLAB is already open close it and reopen. Then you can find ZCU208 device listed in Target Platform selection.

    Hope it helps, it worked for me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer