Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PS SPI directed to PMOD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 731 views
  • Users 0 members are here
Related

PS SPI directed to PMOD

e14 Contributor
e14 Contributor over 13 years ago

Hi guys,

i would like to connect an external chip to the ZEDBOARD and communicate with it using SPI.
I am willing to use the PS PMOD connector for this purpose, so i need to direct the SPI controller to the relevant pins and then write the C code that defines SPI mode.

Is there anywhere where i can find an example for doing this??

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,

    I start using Zedboard few days ago. I'm using Vivado 2013.2 and I have the same problem. Basically, I'd like to connect an LCD dysplay to JE1 connector and drive it through the SPI controller. as I read in other threads, JE1 is a PS PMOD, right? here is my problem: under Vivado I can't redirect the SPI to the PMOD JE1, but only to the MIO pins.
    What am I doing wrong?
    thanks a lot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    maybe I get the solution. as I see in the schematics, JE1 pins are connected to PS_MIO[9:15]; so in Vivado what I see as MIO[10:15] is referred to PS_MIO[10:15], right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    maybe I get the solution. as I see in the schematics, JE1 pins are connected to PS_MIO[9:15]; so in Vivado what I see as MIO[10:15] is referred to PS_MIO[10:15], right?