Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PS SPI directed to PMOD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 729 views
  • Users 0 members are here
Related

PS SPI directed to PMOD

e14 Contributor
e14 Contributor over 13 years ago

Hi guys,

i would like to connect an external chip to the ZEDBOARD and communicate with it using SPI.
I am willing to use the PS PMOD connector for this purpose, so i need to direct the SPI controller to the relevant pins and then write the C code that defines SPI mode.

Is there anywhere where i can find an example for doing this??

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Thank you.
    I plan to do this in the PS only as my PL will have its own code and will probably be busy doing other things such as collecting real time data :)

    I think i understood the steps, i will try to do this on sunday. f i have more questions ill let you know! :)

    thanks

    guys any more example tutorials dont hesitate to post!! :D

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,

    I start using Zedboard few days ago. I'm using Vivado 2013.2 and I have the same problem. Basically, I'd like to connect an LCD dysplay to JE1 connector and drive it through the SPI controller. as I read in other threads, JE1 is a PS PMOD, right? here is my problem: under Vivado I can't redirect the SPI to the PMOD JE1, but only to the MIO pins.
    What am I doing wrong?
    thanks a lot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    maybe I get the solution. as I see in the schematics, JE1 pins are connected to PS_MIO[9:15]; so in Vivado what I see as MIO[10:15] is referred to PS_MIO[10:15], right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    yeah thats right. JE1 is MIO[10:15] + 16,17 i think

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100padudle
    0 100padudle over 12 years ago in reply to e14 Contributor

    Joe,

    What did you decide?  Were you able to control your 16 bit SPI device using the built-in PS SPI controller?

    I am faced with a similar challenge. I have a 16 bit SPI device that uses a 4 wire SPI interface, MISO, MOSI, SCK, CS.  I don't know whether to use the PS SPI controller, an AXI QSPI interface in the PL or just do direct bit banging in software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to 100padudle

    In the followind thread: http://www.zedboard.org/content/sd-card-example-design-using-standalone

    Edh4 has posted his modified zynq_spi_sdc.zip which does bitbanging and is a good example to start with. However bitbanging is slow and you might want to use the PS SPI controller afterward which is basically straightforward although I think a logic analyzer is very handy when writing drivers for this kind of stuff. On this side of the pond, I connected the SD card to the MicroZed PMOD connector.

    QSPI is something else: Quad-SPI has 4 data bit.