Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PS SPI directed to PMOD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 731 views
  • Users 0 members are here
Related

PS SPI directed to PMOD

e14 Contributor
e14 Contributor over 13 years ago

Hi guys,

i would like to connect an external chip to the ZEDBOARD and communicate with it using SPI.
I am willing to use the PS PMOD connector for this purpose, so i need to direct the SPI controller to the relevant pins and then write the C code that defines SPI mode.

Is there anywhere where i can find an example for doing this??

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    yeah thats right. JE1 is MIO[10:15] + 16,17 i think

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    yeah thats right. JE1 is MIO[10:15] + 16,17 i think

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • 100padudle
    0 100padudle over 12 years ago in reply to e14 Contributor

    Joe,

    What did you decide?  Were you able to control your 16 bit SPI device using the built-in PS SPI controller?

    I am faced with a similar challenge. I have a 16 bit SPI device that uses a 4 wire SPI interface, MISO, MOSI, SCK, CS.  I don't know whether to use the PS SPI controller, an AXI QSPI interface in the PL or just do direct bit banging in software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to 100padudle

    In the followind thread: http://www.zedboard.org/content/sd-card-example-design-using-standalone

    Edh4 has posted his modified zynq_spi_sdc.zip which does bitbanging and is a good example to start with. However bitbanging is slow and you might want to use the PS SPI controller afterward which is basically straightforward although I think a logic analyzer is very handy when writing drivers for this kind of stuff. On this side of the pond, I connected the SD card to the MicroZed PMOD connector.

    QSPI is something else: Quad-SPI has 4 data bit.