Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development GPIO PL mapping
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 496 views
  • Users 0 members are here
Related

GPIO PL mapping

e14 Contributor
e14 Contributor over 13 years ago

-
Hi,
in the ZedBoard there is a mapping of LED0-7 and SW0-7 to gpio: 61 to 68 for LEDs and 69 to 76 for switches

Where is this mapping described within the Linux?

And how can I modify SW in order to map the buttons BTNU, BTND... to a gpio such that I can read the status of these buttons in the same way I can read SW0-7?

Where can I read a generic description of these HW/SW topics?

Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Most LED/Button are linked to PL side, unless it is connected the Bank 500 in the ZedBoard schema (page 10).  For example, push button 1, is already connected to MIO 50.  If it's not already connected, you just have to reroute the signal using the constraint file.

    LED and button pins assignment are listed in "Zedboard HW_UG guide."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Most LED/Button are linked to PL side, unless it is connected the Bank 500 in the ZedBoard schema (page 10).  For example, push button 1, is already connected to MIO 50.  If it's not already connected, you just have to reroute the signal using the constraint file.

    LED and button pins assignment are listed in "Zedboard HW_UG guide."